Authentication parameter set.
Public Attributes#
Security key lifetimes.
uint8_t
Reserved, set to zero.
Security protocol trickle timer.
uint8_t
Security protocol trickle max expirations.
uint16_t
Temporary neighbor link minimum timeout (seconds)
Public Attribute Documentation#
key_lifetimes#
sl_wisun_key_lifetimes_params_t sl_wisun_br_params_eapol_s::key_lifetimes
Security key lifetimes.
Definition at line
78
of file /mnt/raid/workspaces/ws.9FtfRPWpI/overlay/gsdk/protocol/wisun/stack/inc/border_router/sl_wisun_br_connection_params_api.h
reserved#
uint8_t sl_wisun_br_params_eapol_s::reserved
Reserved, set to zero.
Definition at line
86
of file /mnt/raid/workspaces/ws.9FtfRPWpI/overlay/gsdk/protocol/wisun/stack/inc/border_router/sl_wisun_br_connection_params_api.h
sec_prot_trickle#
sl_wisun_trickle_params_t sl_wisun_br_params_eapol_s::sec_prot_trickle
Security protocol trickle timer.
Definition at line
80
of file /mnt/raid/workspaces/ws.9FtfRPWpI/overlay/gsdk/protocol/wisun/stack/inc/border_router/sl_wisun_br_connection_params_api.h
sec_prot_trickle_expirations#
uint8_t sl_wisun_br_params_eapol_s::sec_prot_trickle_expirations
Security protocol trickle max expirations.
Definition at line
84
of file /mnt/raid/workspaces/ws.9FtfRPWpI/overlay/gsdk/protocol/wisun/stack/inc/border_router/sl_wisun_br_connection_params_api.h
temp_min_timeout_s#
uint16_t sl_wisun_br_params_eapol_s::temp_min_timeout_s
Temporary neighbor link minimum timeout (seconds)
Definition at line
82
of file /mnt/raid/workspaces/ws.9FtfRPWpI/overlay/gsdk/protocol/wisun/stack/inc/border_router/sl_wisun_br_connection_params_api.h