LFN parameter set.

Public Attributes#

LFN network parameters.

LFN power parameters.

uint32_t

Version of this API.

Public Attribute Documentation#

connection#

sl_wisun_lfn_params_connection_t sl_wisun_lfn_params_t::connection

LFN connection parameters.


Definition at line 128 of file /mnt/raid/workspaces/ws.9FtfRPWpI/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_lfn_params_api.h

data_layer#

sl_wisun_lfn_params_data_layer_t sl_wisun_lfn_params_t::data_layer

LFN data layer parameters.


Definition at line 130 of file /mnt/raid/workspaces/ws.9FtfRPWpI/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_lfn_params_api.h

network#

sl_wisun_lfn_params_network_t sl_wisun_lfn_params_t::network

LFN network parameters.


Definition at line 132 of file /mnt/raid/workspaces/ws.9FtfRPWpI/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_lfn_params_api.h

power#

sl_wisun_lfn_params_power_t sl_wisun_lfn_params_t::power

LFN power parameters.


Definition at line 134 of file /mnt/raid/workspaces/ws.9FtfRPWpI/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_lfn_params_api.h

version#

uint32_t sl_wisun_lfn_params_t::version

Version of this API.

This field allows to store the parameters in an NVM and check on reload that they are compatible with the stack if there was an update.


Definition at line 126 of file /mnt/raid/workspaces/ws.9FtfRPWpI/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_lfn_params_api.h