LFN advanced connection parameters for sl_wisun_set_lfn_advanced_parameters.
Public Attributes#
RFC8415 TX algorithm for DHCP solicitation transmissions.
RFC8415 TX algorithm for EAPOL Key-request transmissions.
Duration for which an LFN waits for a registration confirmation (minutes).
Reserved, set to zero.
Version of sl_wisun_lfn_advanced_parameters_t.
Public Attribute Documentation#
dhcp_solicit_txalg#
sl_wisun_rfc8415_txalg_params_t sl_wisun_lfn_advanced_parameters_t::dhcp_solicit_txalg
RFC8415 TX algorithm for DHCP solicitation transmissions.
key_request_txalg#
sl_wisun_rfc8415_txalg_params_t sl_wisun_lfn_advanced_parameters_t::key_request_txalg
RFC8415 TX algorithm for EAPOL Key-request transmissions.
lfn_na_wait_duration_m#
uint8_t sl_wisun_lfn_advanced_parameters_t::lfn_na_wait_duration_m
Duration for which an LFN waits for a registration confirmation (minutes).
version#
uint32_t sl_wisun_lfn_advanced_parameters_t::version
Version of sl_wisun_lfn_advanced_parameters_t.
Set to SL_WISUN_LFN_ADVANCED_PARAMS_API_VERSION.
Used to identify the layout of the structure when applying advanced LFN parameters. Older supported versions may be accepted and updated internally to the current format, while unsupported versions are rejected.