LFN parent parameter set.
Public Attributes#
Number of broadcast LFN Pan Config retries when LFN Version is incremented Referred to as LFN_MAINTAIN_PARENT_TIME in FAN TPS 1.1.
Duration for which an FFN retransmits DAO on behalf of a registering LFN (minutes).
Interval after which an FFN parent must disable LFN broadcast messaging if the FFN parent is unable communicate with its Border Router.
Public Attribute Documentation#
lfn_lpc_retry_count#
uint8_t sl_wisun_params_lfn_parent_s::lfn_lpc_retry_count
Number of broadcast LFN Pan Config retries when LFN Version is incremented Referred to as LFN_MAINTAIN_PARENT_TIME in FAN TPS 1.1.
256
of file /mnt/raid/workspaces/ws.9FtfRPWpI/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_connection_params_api.h
lfn_na_wait_duration_m#
uint8_t sl_wisun_params_lfn_parent_s::lfn_na_wait_duration_m
Duration for which an FFN retransmits DAO on behalf of a registering LFN (minutes).
This value is administratively configured and should be consistent throughout the network. Make sure that the value is equal to or less than the corresponding field on LFNs. Specification range [30, 120] (set lower for test purposes)
262
of file /mnt/raid/workspaces/ws.9FtfRPWpI/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_connection_params_api.h
lfn_pan_timeout_m#
uint16_t sl_wisun_params_lfn_parent_s::lfn_pan_timeout_m
Interval after which an FFN parent must disable LFN broadcast messaging if the FFN parent is unable communicate with its Border Router.
253
of file /mnt/raid/workspaces/ws.9FtfRPWpI/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_connection_params_api.h