Frequency hopping statistics.
Public Attributes#
int16_t
Estimated clock drift to the parent in microseconds.
uint16_t
Estimated number of hops to the border router based on RPL rank.
int16_t
Deprecated.
uint16_t
Number of seconds since last timing information from the parent.
uint32_t
Deprecated.
uint32_t
Number of times a transmission attempt has failed due to lack of timing information.
Public Attribute Documentation#
drift_compensation#
int16_t sl_wisun_statistics_fhss_t::drift_compensation
Estimated clock drift to the parent in microseconds.
hop_count#
uint16_t sl_wisun_statistics_fhss_t::hop_count
Estimated number of hops to the border router based on RPL rank.
synch_interval#
uint16_t sl_wisun_statistics_fhss_t::synch_interval
Number of seconds since last timing information from the parent.
unknown_neighbor#
uint32_t sl_wisun_statistics_fhss_t::unknown_neighbor
Number of times a transmission attempt has failed due to lack of timing information.