6LoWPAN/IP stack statistics

Public Attributes#

uint16_t

Highest number of frames in the adaptation layer transmission queue.

uint16_t

Current number of frames in the adaptation layer transmission queue.

uint32_t

Number of data buffer allocation attempts.

uint32_t

Number of times data buffer resizing has failed.

uint32_t

Number of times data buffers have been resized due to lack of header space.

uint32_t

Number of times data buffers have been reorganized due to lack of header space.

uint16_t

ETX of the primary parent.

uint16_t

ETX of the secondary parent.

uint32_t

Number of fragmentation errors in received IPv6 packets.

uint32_t

Number of fragmentation errors in transmitted IPv6 packets.

uint32_t

Number of discarded IPv6 packets due to a checksum error.

uint32_t

Number of discarded IPv6 packets due to lack routing information.

uint32_t

Amount of forwarded IPv6 data in bytes.

uint32_t

Number of RPL packet forwarding errors due to inconsistent routing information.

uint32_t

Amount received IPv6 data in bytes.

uint32_t

Number of received IP6 packets.

uint32_t

Number of discarded IPv6 packets during processing.

uint32_t

Amount of transmitted IPv6 data in bytes.

uint32_t

Number of transmitted IPv6 packets.

uint16_t

Number of forwarded MPL messages.

uint16_t

Number of freed MPL messages.

uint16_t

Number of new MPL messages.

uint16_t

Number of deleted MPL messages that were never sent.

uint16_t

Number of received MPL messages.

uint32_t

Number of times a global repair has been triggered by the border router.

uint32_t

Number of times a local repair procedure has been triggered by the node.

uint32_t

Number of discarded RPL packets due to malformed content.

uint32_t

Sum of RPL object sizes that have failed allocation in bytes.

uint32_t

Number of failed RPL transmissions to the parent.

uint32_t

Number of RPL parent changes due to better route cost.

uint32_t

Number of seconds without an RPL parent.

uint32_t

Amount of memory currently allocated for RPL objects in bytes.

uint32_t

Number of discarded RPL packets due to an unknown DODAG instance.

Public Attribute Documentation#

adapt_layer_tx_queue_peak#

uint16_t sl_wisun_statistics_network_t::adapt_layer_tx_queue_peak

Highest number of frames in the adaptation layer transmission queue.


adapt_layer_tx_queue_size#

uint16_t sl_wisun_statistics_network_t::adapt_layer_tx_queue_size

Current number of frames in the adaptation layer transmission queue.


buf_alloc#

uint32_t sl_wisun_statistics_network_t::buf_alloc

Number of data buffer allocation attempts.


buf_headroom_fail#

uint32_t sl_wisun_statistics_network_t::buf_headroom_fail

Number of times data buffer resizing has failed.


buf_headroom_realloc#

uint32_t sl_wisun_statistics_network_t::buf_headroom_realloc

Number of times data buffers have been resized due to lack of header space.


buf_headroom_shuffle#

uint32_t sl_wisun_statistics_network_t::buf_headroom_shuffle

Number of times data buffers have been reorganized due to lack of header space.


etx_1st_parent#

uint16_t sl_wisun_statistics_network_t::etx_1st_parent

ETX of the primary parent.


etx_2nd_parent#

uint16_t sl_wisun_statistics_network_t::etx_2nd_parent

ETX of the secondary parent.


frag_rx_errors#

uint32_t sl_wisun_statistics_network_t::frag_rx_errors

Number of fragmentation errors in received IPv6 packets.


frag_tx_errors#

uint32_t sl_wisun_statistics_network_t::frag_tx_errors

Number of fragmentation errors in transmitted IPv6 packets.


ip_cksum_error#

uint32_t sl_wisun_statistics_network_t::ip_cksum_error

Number of discarded IPv6 packets due to a checksum error.


ip_no_route#

uint32_t sl_wisun_statistics_network_t::ip_no_route

Number of discarded IPv6 packets due to lack routing information.


ip_routed_up#

uint32_t sl_wisun_statistics_network_t::ip_routed_up

Amount of forwarded IPv6 data in bytes.


ip_routeloop_detect#

uint32_t sl_wisun_statistics_network_t::ip_routeloop_detect

Number of RPL packet forwarding errors due to inconsistent routing information.


ip_rx_bytes#

uint32_t sl_wisun_statistics_network_t::ip_rx_bytes

Amount received IPv6 data in bytes.


ip_rx_count#

uint32_t sl_wisun_statistics_network_t::ip_rx_count

Number of received IP6 packets.


ip_rx_drop#

uint32_t sl_wisun_statistics_network_t::ip_rx_drop

Number of discarded IPv6 packets during processing.


ip_tx_bytes#

uint32_t sl_wisun_statistics_network_t::ip_tx_bytes

Amount of transmitted IPv6 data in bytes.


ip_tx_count#

uint32_t sl_wisun_statistics_network_t::ip_tx_count

Number of transmitted IPv6 packets.


mpl_forwarded_messages_count#

uint16_t sl_wisun_statistics_network_t::mpl_forwarded_messages_count

Number of forwarded MPL messages.


mpl_freed_messages_count#

uint16_t sl_wisun_statistics_network_t::mpl_freed_messages_count

Number of freed MPL messages.


mpl_new_messages_count#

uint16_t sl_wisun_statistics_network_t::mpl_new_messages_count

Number of new MPL messages.


mpl_not_tx_count#

uint16_t sl_wisun_statistics_network_t::mpl_not_tx_count

Number of deleted MPL messages that were never sent.


mpl_rx_count#

uint16_t sl_wisun_statistics_network_t::mpl_rx_count

Number of received MPL messages.


rpl_global_repair#

uint32_t sl_wisun_statistics_network_t::rpl_global_repair

Number of times a global repair has been triggered by the border router.


rpl_local_repair#

uint32_t sl_wisun_statistics_network_t::rpl_local_repair

Number of times a local repair procedure has been triggered by the node.


rpl_malformed_message#

uint32_t sl_wisun_statistics_network_t::rpl_malformed_message

Number of discarded RPL packets due to malformed content.


rpl_memory_overflow#

uint32_t sl_wisun_statistics_network_t::rpl_memory_overflow

Sum of RPL object sizes that have failed allocation in bytes.


rpl_parent_tx_fail#

uint32_t sl_wisun_statistics_network_t::rpl_parent_tx_fail

Number of failed RPL transmissions to the parent.


rpl_route_routecost_better_change#

uint32_t sl_wisun_statistics_network_t::rpl_route_routecost_better_change

Number of RPL parent changes due to better route cost.


rpl_time_no_next_hop#

uint32_t sl_wisun_statistics_network_t::rpl_time_no_next_hop

Number of seconds without an RPL parent.


rpl_total_memory#

uint32_t sl_wisun_statistics_network_t::rpl_total_memory

Amount of memory currently allocated for RPL objects in bytes.


rpl_unknown_instance#

uint32_t sl_wisun_statistics_network_t::rpl_unknown_instance

Number of discarded RPL packets due to an unknown DODAG instance.