Advanced RPL parameters for sl_wisun_set_ffn_advanced_parameters.

Public Attributes#

RFC8415 TX algorithm parameters for DAO transmission rand specification range [0.0, 1.0] irt_s specification range [1, 60] mrt_s specification range [0, 600] mrd_s specification range [0, 3600] mrc specification range [0, 15].

uint16_t

Maximum delay before sending an ETX probe (seconds).

uint16_t

Maximum delay before sending the first RPL DIS (unicast/multicast) packet following transition to Join State 4 - Preferred Parent Selection (seconds)

Public Attribute Documentation#

dao_txalg#

sl_wisun_rfc8415_txalg_params_t sl_wisun_ffn_advanced_rpl_params_t::dao_txalg

RFC8415 TX algorithm parameters for DAO transmission rand specification range [0.0, 1.0] irt_s specification range [1, 60] mrt_s specification range [0, 600] mrd_s specification range [0, 3600] mrc specification range [0, 15].


etx_probe_max_delay_s#

uint16_t sl_wisun_ffn_advanced_rpl_params_t::etx_probe_max_delay_s

Maximum delay before sending an ETX probe (seconds).


first_dis_max_delay_s#

uint16_t sl_wisun_ffn_advanced_rpl_params_t::first_dis_max_delay_s

Maximum delay before sending the first RPL DIS (unicast/multicast) packet following transition to Join State 4 - Preferred Parent Selection (seconds)