Event Manager#
Enumerations#
System events.
Button events.
Functions#
Initializes event scheduler.
Adds a given event to the event queue.
Processes events.
Adds a given event to the job queue.
Deque job queue.
Get number of events on queue.
Macros#
Event groups for application state event machine.
Event group for keys 0x40 - 0x6F.
Event group for zaf 0x80 - 0xFF.
Enumeration Documentation#
_EVENT_SYSTEM_#
_EVENT_SYSTEM_
System events.
| Enumerator | |
|---|---|
| EVENT_SYSTEM_RESET | |
| EVENT_SYSTEM_LEARNMODE_START | |
| EVENT_SYSTEM_LEARNMODE_FINISHED | |
| EVENT_SYSTEM_LEARNMODE_STOP | |
| EVENT_SYSTEM_LEARNMODE_TOGGLE | |
| EVENT_SYSTEM_WATCHDOG_RESET | |
| EVENT_SYSTEM_OTA_START | |
| EVENT_SYSTEM_LEARNMODE_DSK_START | |
| EVENT_SYSTEM_FLUSHMEM_READY | |
| EVENT_SYSTEM_SMARTSTART_IN_PROGRESS | |
| EVENT_SYSTEM_EMPTY | |
_BUTTON_EVENT_
_BUTTON_EVENT_
Button events.
NB: For every button there MUST be the following events in this order: DOWN, UP, SHORT_PRESS, HOLD, LONG_PRESS The macros BTN_EVENT_xxx in board.h depends on it.
| Enumerator | |
|---|---|
| EVENT_PB1_DOWN | |
| EVENT_PB1_UP | |
| EVENT_PB1_SHORT_PRESS | |
| EVENT_PB1_HOLD | |
| EVENT_PB1_LONG_PRESS | |
| EVENT_PB2_DOWN | |
| EVENT_PB2_UP | |
| EVENT_PB2_SHORT_PRESS | |
| EVENT_PB2_HOLD | |
| EVENT_PB2_LONG_PRESS | |
| EVENT_PB3_DOWN | |
| EVENT_PB3_UP | |
| EVENT_PB3_SHORT_PRESS | |
| EVENT_PB3_HOLD | |
| EVENT_PB3_LONG_PRESS | |
| EVENT_PB4_DOWN | |
| EVENT_PB4_UP | |
| EVENT_PB4_SHORT_PRESS | |
| EVENT_PB4_HOLD | |
| EVENT_PB4_LONG_PRESS | |
| EVENT_PB5_DOWN | |
| EVENT_PB5_UP | |
| EVENT_PB5_SHORT_PRESS | |
| EVENT_PB5_HOLD | |
| EVENT_PB5_LONG_PRESS | |
| EVENT_PB6_DOWN | |
| EVENT_PB6_UP | |
| EVENT_PB6_SHORT_PRESS | |
| EVENT_PB6_HOLD | |
| EVENT_PB6_LONG_PRESS | |
| EVENT_SLIDER1_DOWN | |
| EVENT_SLIDER1_UP | |
| EVENT_SLIDER1_SHORT_PRESS | |
| EVENT_SLIDER1_HOLD | |
| EVENT_SLIDER1_LONG_PRESS | |
| EVENT_BTN_MAX | EVENT_BTN_MAX define the last enum type. |
Typedef Documentation#
BUTTON_EVENT
typedef enum _BUTTON_EVENT_ BUTTON_EVENT
Button events.
NB: For every button there MUST be the following events in this order: DOWN, UP, SHORT_PRESS, HOLD, LONG_PRESS The macros BTN_EVENT_xxx in board.h depends on it.
Function Documentation#
ZAF_eventSchedulerInit#
void ZAF_eventSchedulerInit (void(*)(uint8_t) pApplicationStateMachine)
Initializes event scheduler.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void(*)(uint8_t) | N/A | pApplicationStateMachine |
ZCB_eventSchedulerEventAdd#
bool ZCB_eventSchedulerEventAdd (uint8_t event)
Adds a given event to the event queue.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | N/A | event | A given event. |
Returns
true if given event is added to queue, false if queue full.
ZCB_eventScheduler#
bool ZCB_eventScheduler (void )
Processes events.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
ZAF_jobEnqueue#
bool ZAF_jobEnqueue (uint8_t event)
Adds a given event to the job queue.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | N/A | event | A given event. |
Returns
true if given event is added to queue, false if queue full.
ZAF_jobDequeue#
bool ZAF_jobDequeue (uint8_t * pEvent)
Deque job queue.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t * | [out] | pEvent | return event from the queue. |
Returns
false if queue is empty else true.
ZAF_jobQueueCount#
uint8_t ZAF_jobQueueCount (void )
Get number of events on queue.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
number of events on queue