Application Timer#
Modules#
Functions#
Initialize AppTimer.
Configures the Receiver task of callbacks.
Register a SwTimer to a TimerLiaison.
Wrapper for AppTimerRegister to register timers that should be re-loaded after deep sleep hibernate.
Wrapper for TimerStart() that ensures the timer value is saved so it can be re-loaded after deep sleep hibernate.
Wrapper for TimerRestart() that ensures the timer status is saved so it can be re-loaded after deep sleep hibernate.
Wrapper for TimerStop() that ensures the timer status is saved so it does not get re-started after deep sleep hibernate.
Must be called from application task when the task notification bit assigned to AppTimer is set.
Clear storage used for persisting application timers during deep sleep hibernate.
Save SSwTimers that should survive deep sleep Hibernate.
Load SSwTimers after deep sleep hibernate wakeup.
Get index of first retention register used for saving Deep Sleep persistent app timers.
Get index of last retention register used for saving Deep Sleep persistent app timers.
Stops all the running applications timers.
Macros#
Max number of application timers.
Function Documentation#
AppTimerInit#
void AppTimerInit (uint8_t iTaskNotificationBitNumber, void * ReceiverTask)
Initialize AppTimer.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | [in] | iTaskNotificationBitNumber | Number defines which bit to use when notifying receiver task of pending timer event (range 0 - 31) |
| void * | [in] | ReceiverTask | Handle to the Application task |
AppTimerSetReceiverTask#
void AppTimerSetReceiverTask (void * ReceiverTask)
Configures the Receiver task of callbacks.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void * | [in] | ReceiverTask | Handle to the Application task |
Provided as the AppTimer may be needed for registering SwTimers before the receiver task is created, meaning AppTimerInit is called prior to the Receiver task handle being available. Though not the intention, the receiver task can be changed at run time.
AppTimerRegister#
bool AppTimerRegister (SSwTimer * pTimer, bool bAutoReload, void(*)(SSwTimer *pTimer) pCallback)
Register a SwTimer to a TimerLiaison.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| SSwTimer * | [in] | pTimer | Pointer to the SwTimer object to register |
| bool | [in] | bAutoReload | Enable timer auto reload on timeout. Configuration of AutoReload cannot be changed after registration. |
| void(*)(SSwTimer *pTimer) | [in] | pCallback | Callback method of type void Callback(SSwTimer* pTimer). Argument may be NULL, in which case no callback is performed. |
Initial SwTimer configuration is also performed.
Method creates a static FreeRTOS timer from the SwTimer object passed as argument, and registers it as requiring callbacks in the Receiver task. If calling method AppTimerRegister on the same SwTimer object multiple times, all but the first call will be ignored.
AppTimerDeepSleepPersistentRegister#
bool AppTimerDeepSleepPersistentRegister (SSwTimer * pTimer, bool bAutoReload, void(*)(SSwTimer *pTimer) pCallback)
Wrapper for AppTimerRegister to register timers that should be re-loaded after deep sleep hibernate.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| SSwTimer * | N/A | pTimer | |
| bool | N/A | bAutoReload | |
| void(*)(SSwTimer *pTimer) | N/A | pCallback |
In addition to having AppTimerRegister() register the timer with a TimerLiaison this function also marks the timer to survive deep sleep hibernate.
For parameter descriptions See Also
AppTimerDeepSleepPersistentStart#
ESwTimerStatus AppTimerDeepSleepPersistentStart (SSwTimer * pTimer, uint32_t iTimeout)
Wrapper for TimerStart() that ensures the timer value is saved so it can be re-loaded after deep sleep hibernate.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| SSwTimer * | N/A | pTimer | |
| uint32_t | N/A | iTimeout |
For parameter descriptions See Also
AppTimerDeepSleepPersistentRestart#
ESwTimerStatus AppTimerDeepSleepPersistentRestart (SSwTimer * pTimer)
Wrapper for TimerRestart() that ensures the timer status is saved so it can be re-loaded after deep sleep hibernate.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| SSwTimer * | N/A | pTimer |
For parameter descriptions See Also
AppTimerDeepSleepPersistentStop#
ESwTimerStatus AppTimerDeepSleepPersistentStop (SSwTimer * pTimer)
Wrapper for TimerStop() that ensures the timer status is saved so it does not get re-started after deep sleep hibernate.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| SSwTimer * | N/A | pTimer |
For parameter descriptions See Also
AppTimerNotificationHandler#
void AppTimerNotificationHandler (void )
Must be called from application task when the task notification bit assigned to AppTimer is set.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Method will perform pending callbacks. There is no side effects from calling method when assigned task notification bit was not set.
AppTimerDeepSleepPersistentResetStorage#
void AppTimerDeepSleepPersistentResetStorage (void )
Clear storage used for persisting application timers during deep sleep hibernate.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
AppTimerDeepSleepPersistentSaveAll#
void AppTimerDeepSleepPersistentSaveAll (void )
Save SSwTimers that should survive deep sleep Hibernate.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
The number of remaining milliseconds until timeout are saved to the RTCC retention registers for all application timers registered to be persisted during Deep Sleep.
AppTimerDeepSleepPersistentLoadAll#
void AppTimerDeepSleepPersistentLoadAll (EResetReason_t resetReason)
Load SSwTimers after deep sleep hibernate wakeup.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| EResetReason_t | N/A | resetReason | Reason why the device woke up |
Activates callback registered for the timer causing the wakeup
Must be called AFTER AppTimerInit() and AppTimerDeepSleepPersistentRegister()
AppTimerDeepSleepGetFirstRetentionRegister#
uint32_t AppTimerDeepSleepGetFirstRetentionRegister (void )
Get index of first retention register used for saving Deep Sleep persistent app timers.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
The retention registers are manipulated with the zpal_retention_register_xx() API.
AppTimerDeepSleepGetLastRetentionRegister#
uint32_t AppTimerDeepSleepGetLastRetentionRegister (void )
Get index of last retention register used for saving Deep Sleep persistent app timers.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
NB: The number of retention registers used depends on how many times AppTimerDeepSleepPersistentRegister() have been called since system startup. It is not safe to use the returned value to locate "free" retention registers unless it is guarantees that all calls to AppTimerDeepSleepPersistentRegister() has been performed.
The retention registers are manipulated with the zpal_retention_register_xx() API.
AppTimerStopAll#
void AppTimerStopAll (void )
Stops all the running applications timers.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |