Transmit options for ZW_SendDataEx.

Public Attributes#

< Destination node ID - 0xFF == all nodes

Transmit options.

Options for enabling specific Security scheme functionality.

uint8_t

Security key to use for sending.

More transmit options.

uint8_t

Public Attribute Documentation#

destNode#

node_id_t _TRANSMIT_OPTIONS_TYPE::destNode

< Destination node ID - 0xFF == all nodes

Reserved


Definition at line 216 of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_transport_api.h

bSrcNode#

node_id_t _TRANSMIT_OPTIONS_TYPE::bSrcNode

Transmit options.


Definition at line 218 of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_transport_api.h

txOptions#

TxOptions_t _TRANSMIT_OPTIONS_TYPE::txOptions

Options for enabling specific Security scheme functionality.


Definition at line 220 of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_transport_api.h

txSecOptions#

uint8_t _TRANSMIT_OPTIONS_TYPE::txSecOptions

Security key to use for sending.


Definition at line 222 of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_transport_api.h

securityKey#

enum SECURITY_KEY _TRANSMIT_OPTIONS_TYPE::securityKey

More transmit options.


Definition at line 224 of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_transport_api.h

txOptions2#

uint8_t _TRANSMIT_OPTIONS_TYPE::txOptions2

Definition at line 226 of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_transport_api.h