Public Attributes#

uint32_t

Passed 1ms ticks.

uint8_t

Repeaters in route, zero for direct range.

struct s_rssi_val

rssi_values per hop for direct and routed frames.

Public Attribute Documentation#

TransmitTicks#

uint32_t _TX_STATUS_TYPE_::TransmitTicks

Passed 1ms ticks.


Definition at line 141 of file /mnt/raid/workspaces/ws.Mh9rMZz8x/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_transport_api.h

bRepeaters#

uint8_t _TX_STATUS_TYPE_::bRepeaters

Repeaters in route, zero for direct range.


Definition at line 142 of file /mnt/raid/workspaces/ws.Mh9rMZz8x/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_transport_api.h

rssi_values#

struct s_rssi_val _TX_STATUS_TYPE_::rssi_values

rssi_values per hop for direct and routed frames.

Contains repeaters + 1 values.


Definition at line 145 of file /mnt/raid/workspaces/ws.Mh9rMZz8x/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_transport_api.h

bACKChannelNo#

uint8_t _TX_STATUS_TYPE_::bACKChannelNo

Definition at line 146 of file /mnt/raid/workspaces/ws.Mh9rMZz8x/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_transport_api.h

bLastTxChannelNo#

uint8_t _TX_STATUS_TYPE_::bLastTxChannelNo

Definition at line 147 of file /mnt/raid/workspaces/ws.Mh9rMZz8x/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_transport_api.h

bRouteSchemeState#

uint8_t _TX_STATUS_TYPE_::bRouteSchemeState

Definition at line 148 of file /mnt/raid/workspaces/ws.Mh9rMZz8x/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_transport_api.h

pLastUsedRoute#

uint8_t _TX_STATUS_TYPE_::pLastUsedRoute[LAST_USED_ROUTE_SIZE]

Definition at line 149 of file /mnt/raid/workspaces/ws.Mh9rMZz8x/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_transport_api.h

bRouteTries#

uint8_t _TX_STATUS_TYPE_::bRouteTries

Definition at line 150 of file /mnt/raid/workspaces/ws.Mh9rMZz8x/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_transport_api.h

bLastFailedLink#

S_ROUTE_LINK_T _TX_STATUS_TYPE_::bLastFailedLink

Definition at line 151 of file /mnt/raid/workspaces/ws.Mh9rMZz8x/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_transport_api.h

bUsedTxpower#

int8_t _TX_STATUS_TYPE_::bUsedTxpower

Definition at line 152 of file /mnt/raid/workspaces/ws.Mh9rMZz8x/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_transport_api.h

bMeasuredNoiseFloor#

int8_t _TX_STATUS_TYPE_::bMeasuredNoiseFloor

Definition at line 153 of file /mnt/raid/workspaces/ws.Mh9rMZz8x/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_transport_api.h

bDestinationAckUsedTxPower#

int8_t _TX_STATUS_TYPE_::bDestinationAckUsedTxPower

Definition at line 154 of file /mnt/raid/workspaces/ws.Mh9rMZz8x/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_transport_api.h

bDestinationAckMeasuredRSSI#

int8_t _TX_STATUS_TYPE_::bDestinationAckMeasuredRSSI

Definition at line 155 of file /mnt/raid/workspaces/ws.Mh9rMZz8x/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_transport_api.h

bDestinationAckMeasuredNoiseFloor#

int8_t _TX_STATUS_TYPE_::bDestinationAckMeasuredNoiseFloor

Definition at line 156 of file /mnt/raid/workspaces/ws.Mh9rMZz8x/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_transport_api.h