Network statistics structure.

Public Attributes#

uint32_t

Transmitted Frames.

uint32_t

LBT backoffs.

uint32_t

Received Frames (No errors).

uint32_t

Checksum Errors.

uint32_t

CRC16 Errors.

uint32_t

Foreign Home ID.

uint32_t

Accumulated transmission time in ms for channel 0.

Public Attribute Documentation#

tx_frames#

uint32_t zpal_radio_network_stats_t::tx_frames

Transmitted Frames.


Definition at line 474 of file /mnt/raid/workspaces/ws.Mh9rMZz8x/overlay/gsdk/protocol/z-wave/PAL/inc/zpal_radio.h

tx_lbt_back_offs#

uint32_t zpal_radio_network_stats_t::tx_lbt_back_offs

LBT backoffs.


Definition at line 475 of file /mnt/raid/workspaces/ws.Mh9rMZz8x/overlay/gsdk/protocol/z-wave/PAL/inc/zpal_radio.h

rx_frames#

uint32_t zpal_radio_network_stats_t::rx_frames

Received Frames (No errors).


Definition at line 476 of file /mnt/raid/workspaces/ws.Mh9rMZz8x/overlay/gsdk/protocol/z-wave/PAL/inc/zpal_radio.h

rx_lrc_errors#

uint32_t zpal_radio_network_stats_t::rx_lrc_errors

Checksum Errors.


Definition at line 477 of file /mnt/raid/workspaces/ws.Mh9rMZz8x/overlay/gsdk/protocol/z-wave/PAL/inc/zpal_radio.h

rx_crc_errors#

uint32_t zpal_radio_network_stats_t::rx_crc_errors

CRC16 Errors.


Definition at line 478 of file /mnt/raid/workspaces/ws.Mh9rMZz8x/overlay/gsdk/protocol/z-wave/PAL/inc/zpal_radio.h

rx_foreign_home_id#

uint32_t zpal_radio_network_stats_t::rx_foreign_home_id

Foreign Home ID.


Definition at line 479 of file /mnt/raid/workspaces/ws.Mh9rMZz8x/overlay/gsdk/protocol/z-wave/PAL/inc/zpal_radio.h

tx_time_channel#

uint32_t zpal_radio_network_stats_t::tx_time_channel[ZPAL_RADIO_ZWAVE_CHANNEL_NUM]

Accumulated transmission time in ms for channel 0.


Definition at line 480 of file /mnt/raid/workspaces/ws.Mh9rMZz8x/overlay/gsdk/protocol/z-wave/PAL/inc/zpal_radio.h