Parameters required when transmitting a frame.

Public Attributes#

Channel Speed to use when transmitting a frame.

Channel id to use when transmitting a frame.

CRC Type to use. XOR is used in 2 channel at 9600 and 40k baud rate. CRC CCITT is used in 100k frames.

uint8_t

The byte value used for the preamble sequence.

uint8_t

Length of the preamble. Minimum preamble length is specified in ITU G.9959-2015.

uint8_t

The start of frame byte used to indicate the end of preamble and the start of frame.

uint8_t

Number of repetitions for the frame. This is used for wakeup beams where the beam is to be repeated for 250 or 1000 ms.

Public Attribute Documentation#

speed#

zpal_radio_speed_t zpal_radio_transmit_parameter_t::speed

Channel Speed to use when transmitting a frame.


Definition at line 385 of file /mnt/raid/workspaces/ws.Mh9rMZz8x/overlay/gsdk/protocol/z-wave/PAL/inc/zpal_radio.h

channel_id#

zpal_radio_zwave_channel_t zpal_radio_transmit_parameter_t::channel_id

Channel id to use when transmitting a frame.


Definition at line 386 of file /mnt/raid/workspaces/ws.Mh9rMZz8x/overlay/gsdk/protocol/z-wave/PAL/inc/zpal_radio.h

crc#

zpal_radio_crc_t zpal_radio_transmit_parameter_t::crc

CRC Type to use. XOR is used in 2 channel at 9600 and 40k baud rate. CRC CCITT is used in 100k frames.


Definition at line 387 of file /mnt/raid/workspaces/ws.Mh9rMZz8x/overlay/gsdk/protocol/z-wave/PAL/inc/zpal_radio.h

preamble#

uint8_t zpal_radio_transmit_parameter_t::preamble

The byte value used for the preamble sequence.


Definition at line 388 of file /mnt/raid/workspaces/ws.Mh9rMZz8x/overlay/gsdk/protocol/z-wave/PAL/inc/zpal_radio.h

preamble_length#

uint8_t zpal_radio_transmit_parameter_t::preamble_length

Length of the preamble. Minimum preamble length is specified in ITU G.9959-2015.


Definition at line 389 of file /mnt/raid/workspaces/ws.Mh9rMZz8x/overlay/gsdk/protocol/z-wave/PAL/inc/zpal_radio.h

start_of_frame#

uint8_t zpal_radio_transmit_parameter_t::start_of_frame

The start of frame byte used to indicate the end of preamble and the start of frame.


Definition at line 390 of file /mnt/raid/workspaces/ws.Mh9rMZz8x/overlay/gsdk/protocol/z-wave/PAL/inc/zpal_radio.h

repeats#

uint8_t zpal_radio_transmit_parameter_t::repeats

Number of repetitions for the frame. This is used for wakeup beams where the beam is to be repeated for 250 or 1000 ms.


Definition at line 391 of file /mnt/raid/workspaces/ws.Mh9rMZz8x/overlay/gsdk/protocol/z-wave/PAL/inc/zpal_radio.h