Common#
Functions#
cc_engine_multicast_request(const AGI_PROFILE *pProfile, uint8_t endpoint, CMD_CLASS_GRP *pcmdGrp, uint8_t *pPayload, uint8_t size, uint8_t fSupervisionEnable, void(*pCbFunc)(TRANSMISSION_RESULT *pTransmissionResult))
Initiates the transmission of a multicast request.
Function Documentation#
cc_engine_multicast_request#
JOB_STATUS cc_engine_multicast_request (const AGI_PROFILE * pProfile, uint8_t endpoint, CMD_CLASS_GRP * pcmdGrp, uint8_t * pPayload, uint8_t size, uint8_t fSupervisionEnable, void(*)(TRANSMISSION_RESULT *pTransmissionResult) pCbFunc)
Initiates the transmission of a multicast request.
Parameters
[in] | pProfile | pointer to AGI profile or NULL for lifeline |
[in] | endpoint | source endpoint |
[in] | pcmdGrp | command class and command |
[in] | pPayload | payload |
[in] | size | size of payload |
[in] | fSupervisionEnable | enable or not supervision |
[in] | pCbFunc | Callback function to be called when transmission is done/failed. |
Returns
JOB_STATUS Status of the job.
Definition at line
33
of file /mnt/raid/workspaces/ws.6QOxxjIBR/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/Common/CC_Common.h