Transmit Options#

Transmit frame option flags.

Macros#

#define
TRANSMIT_OPTION_ACK 0x01

Request acknowledge from destination node.

#define
TRANSMIT_OPTION_LOW_POWER 0x02

Rransmit at low output power level (1/3 of normal RF range)

#define
TRANSMIT_OPTION_MULTICAST_AS_BROADCAST 0x02

The multicast frame should be send as a broadcast.

#define
TRANSMIT_OPTION_AUTO_ROUTE 0x04

Request retransmission via repeater nodes.

#define
TRANSMIT_OPTION_NO_ROUTE 0x10

Do not use response route - Even if available.

#define
TRANSMIT_OPTION_EXPLORE 0x20

Use explore frame if needed.