Public Attributes#
uint8_t
uint8_t 1, bit 0-6 - Can represent endpoints from 1-127 unless used as a bitmask where endpoint 1-7 is represented.
uint8_t
uint8_t 1, bit 7 - Reserved
Public Attribute Documentation#
nodeId#
node_id_t _MULTICHAN_SOURCE_NODE_ID_::nodeId
The ID of the source node.
Definition at line
27
of file /mnt/raid/workspaces/ws.ZFSvPe7ik/overlay/gsdk/protocol/z-wave/ZAF/ApplicationUtilities/ZAF_types.h
endpoint#
uint8_t _MULTICHAN_SOURCE_NODE_ID_::endpoint
uint8_t 1, bit 0-6 - Can represent endpoints from 1-127 unless used as a bitmask where endpoint 1-7 is represented.
Definition at line
30
of file /mnt/raid/workspaces/ws.ZFSvPe7ik/overlay/gsdk/protocol/z-wave/ZAF/ApplicationUtilities/ZAF_types.h
res#
uint8_t _MULTICHAN_SOURCE_NODE_ID_::res
uint8_t 1, bit 7 - Reserved
Definition at line
32
of file /mnt/raid/workspaces/ws.ZFSvPe7ik/overlay/gsdk/protocol/z-wave/ZAF/ApplicationUtilities/ZAF_types.h