Per-channel jamming detection configuration.

Public Attributes#

int8_t

RSSI threshold in dBm; samples above this threshold are counted as high.

uint8_t

Number of samples in the window that triggers jamming event (e.g.

Public Attribute Documentation#

rssi_threshold_dbm#

int8_t sl_jamming_detection_channel_config_t::rssi_threshold_dbm

RSSI threshold in dBm; samples above this threshold are counted as high.


critical_number_of_samples#

uint8_t sl_jamming_detection_channel_config_t::critical_number_of_samples

Number of samples in the window that triggers jamming event (e.g.

95 or more samples in the 15 s window will be reported as jammed).