Configuration for the jamming detection algorithm.

Samples are taken every 100 ms over a fixed window (e.g. 150 samples = 15 s). A channel is reported jammed when at least samples_per_channel samples in the window are above the RSSI threshold.

Public Attributes#

uint16_t

Seconds between periodic jamming reports; 0 disables periodic reporting ([0,20]).

Callback invoked when jamming is detected on one or more channels.

Callback invoked when RSSI collection is ready.

Public Attribute Documentation#

settings#

sl_jamming_detection_channel_config_t sl_jamming_detection_config_t::settings[SL_JAMMING_DETECTION_NUM_STATS_CHANNELS]

report_interval_sec#

uint16_t sl_jamming_detection_config_t::report_interval_sec

Seconds between periodic jamming reports; 0 disables periodic reporting ([0,20]).


report_callback#

sl_jamming_detection_report_callback_t sl_jamming_detection_config_t::report_callback

Callback invoked when jamming is detected on one or more channels.


collection_callback#

sl_jamming_detection_collection_callback_t sl_jamming_detection_config_t::collection_callback

Callback invoked when RSSI collection is ready.