Per-channel jamming detection statistics.

Public Attributes#

int8_t

RSSI threshold in dBm for this channel.

uint8_t

number of samples above threshold to trigger jamming detection.

uint8_t

Number of samples above threshold in the window.

Public Attribute Documentation#

rssi_threshold_dbm#

int8_t sl_jamming_detection_channel_statistics_t::rssi_threshold_dbm

RSSI threshold in dBm for this channel.


critical_number_of_samples#

uint8_t sl_jamming_detection_channel_statistics_t::critical_number_of_samples

number of samples above threshold to trigger jamming detection.


samples_above_threshold#

uint8_t sl_jamming_detection_channel_statistics_t::samples_above_threshold

Number of samples above threshold in the window.