TimerLiaison object.
All content is private.
Public Attributes#
uint32_t
uint8_t
Keeps count of added timers.
uint8_t
Size of pTimerList.
struct SSwTimer **
Pointer to array of pointers to SwTimer objects.
uint8_t
which bit to use when notifying receiver task of pending timer event(range 0 - 31)
void *
Handle to task in which callbacks should be performed.
Public Attribute Documentation#
dummy#
uint32_t SSwTimerLiaison::dummy[PRIVATE_STATIC_TIMER_SIZE]
Definition at line
94
of file /mnt/raid/workspaces/ws.6QOxxjIBR/overlay/gsdk/protocol/z-wave/Components/SwTimer/SwTimerLiaison.h
iTimerCount#
uint8_t SSwTimerLiaison::iTimerCount
Keeps count of added timers.
Definition at line
95
of file /mnt/raid/workspaces/ws.6QOxxjIBR/overlay/gsdk/protocol/z-wave/Components/SwTimer/SwTimerLiaison.h
iTimerListSize#
uint8_t SSwTimerLiaison::iTimerListSize
Size of pTimerList.
Definition at line
96
of file /mnt/raid/workspaces/ws.6QOxxjIBR/overlay/gsdk/protocol/z-wave/Components/SwTimer/SwTimerLiaison.h
pTimerList#
struct SSwTimer** SSwTimerLiaison::pTimerList
Pointer to array of pointers to SwTimer objects.
Definition at line
97
of file /mnt/raid/workspaces/ws.6QOxxjIBR/overlay/gsdk/protocol/z-wave/Components/SwTimer/SwTimerLiaison.h
iTaskNotificationBitNumber#
uint8_t SSwTimerLiaison::iTaskNotificationBitNumber
which bit to use when notifying receiver task of pending timer event(range 0 - 31)
Definition at line
98
of file /mnt/raid/workspaces/ws.6QOxxjIBR/overlay/gsdk/protocol/z-wave/Components/SwTimer/SwTimerLiaison.h
ReceiverTask#
void* SSwTimerLiaison::ReceiverTask
Handle to task in which callbacks should be performed.
Definition at line
100
of file /mnt/raid/workspaces/ws.6QOxxjIBR/overlay/gsdk/protocol/z-wave/Components/SwTimer/SwTimerLiaison.h