Z-Wave receive frame.
Public Attributes#
Parameters for the received frame.
uint8_t
Length of payload following this frame.
uint8_t
Array with complete frame data received.
Public Attribute Documentation#
rx_parameters#
zpal_radio_rx_parameters_t zpal_radio_receive_frame_t::rx_parameters
Parameters for the received frame.
frame_content_length#
uint8_t zpal_radio_receive_frame_t::frame_content_length
Length of payload following this frame.
frame_content#
uint8_t zpal_radio_receive_frame_t::frame_content[ZWAVE_MAXIMUM_PAYLOAD_SIZE_LR]
Array with complete frame data received.