Parameters required when transmitting a frame.
Public Attributes#
Channel Speed to use when transmitting a frame.
Channel id to use when transmitting a frame.
CRC Type to use. XOR is used in 2 channel at 9600 and 40k baud rate. CRC CCITT is used in 100k frames.
The byte value used for the preamble sequence.
Length of the preamble. Minimum preamble length is specified in ITU G.9959-2015.
The start of frame byte used to indicate the end of preamble and the start of frame.
Number of repetitions for the frame. This is used for wakeup beams where the beam is to be repeated for 250 or 1000 ms.
1 to transmit frame with LBT, 0 without LBT
Timestamp (in zpal base time) that must be used as reference for the Rx-To-Tx turnaround time.
Public Attribute Documentation#
speed#
zpal_radio_speed_t zpal_radio_transmit_parameter_t::speed
Channel Speed to use when transmitting a frame.
channel_id#
zpal_radio_zwave_channel_t zpal_radio_transmit_parameter_t::channel_id
Channel id to use when transmitting a frame.
crc#
zpal_radio_crc_t zpal_radio_transmit_parameter_t::crc
CRC Type to use. XOR is used in 2 channel at 9600 and 40k baud rate. CRC CCITT is used in 100k frames.
preamble#
uint8_t zpal_radio_transmit_parameter_t::preamble
The byte value used for the preamble sequence.
preamble_length#
uint8_t zpal_radio_transmit_parameter_t::preamble_length
Length of the preamble. Minimum preamble length is specified in ITU G.9959-2015.
start_of_frame#
uint8_t zpal_radio_transmit_parameter_t::start_of_frame
The start of frame byte used to indicate the end of preamble and the start of frame.
repeats#
uint8_t zpal_radio_transmit_parameter_t::repeats
Number of repetitions for the frame. This is used for wakeup beams where the beam is to be repeated for 250 or 1000 ms.
turnaround_ref_tick#
zpal_time_t zpal_radio_transmit_parameter_t::turnaround_ref_tick
Timestamp (in zpal base time) that must be used as reference for the Rx-To-Tx turnaround time.
Mostly used for Ack. If not 0, the zpal must guarantee the minimum Rx-To-Tx turnaround time before the Tx. Not done with the TxQueue delay because:
TxQueue delay is 1ms base time which is not enough (Rx-to-Tx turnaround time is 1ms)
Ack is high priority and should "lock" the TxQueue without any delay (TxQueue delay is handled before adding the frame to the TxQueue).