This describes a one of several different types of keys and its associated data.

Public Attribute Documentation#

bitmask#

EmberKeyStructBitmask EmberKeyStruct::bitmask

This bitmask indicates whether various fields in the structure contain valid data. It also contains the index of the network the key belongs to.


Definition at line 2184 of file ./stack/include/ember-types.h

type#

EmberKeyType EmberKeyStruct::type

This indicates the type of the security key.


Definition at line 2186 of file ./stack/include/ember-types.h

key#

EmberKeyData EmberKeyStruct::key

This is the actual key data.


Definition at line 2188 of file ./stack/include/ember-types.h

Referenced by printKeyInfo , and printKeyTable

outgoingFrameCounter#

uint32_t EmberKeyStruct::outgoingFrameCounter

This is the outgoing frame counter associated with the key. It will contain valid data based on the EmberKeyStructBitmask.


Definition at line 2191 of file ./stack/include/ember-types.h

incomingFrameCounter#

uint32_t EmberKeyStruct::incomingFrameCounter

This is the incoming frame counter associated with the key. It will contain valid data based on the EmberKeyStructBitmask.


Definition at line 2194 of file ./stack/include/ember-types.h

sequenceNumber#

uint8_t EmberKeyStruct::sequenceNumber

This is the sequence number associated with the key. It will contain valid data based on the EmberKeyStructBitmask.


Definition at line 2197 of file ./stack/include/ember-types.h

partnerEUI64#

EmberEUI64 EmberKeyStruct::partnerEUI64

This is the Partner EUI64 associated with the key. It will contain valid data based on the EmberKeyStructBitmask.


Definition at line 2200 of file ./stack/include/ember-types.h