This data structure contains the transient key data that is used during Zigbee 3.0 joining.

Public Attribute Documentation#

eui64#

EmberEUI64 EmberTransientKeyData::eui64

Definition at line 2151 of file ./stack/include/ember-types.h

keyData#

EmberKeyData EmberTransientKeyData::keyData

Definition at line 2152 of file ./stack/include/ember-types.h

incomingFrameCounter#

uint32_t EmberTransientKeyData::incomingFrameCounter

Definition at line 2153 of file ./stack/include/ember-types.h

bitmask#

EmberKeyStructBitmask EmberTransientKeyData::bitmask

Definition at line 2154 of file ./stack/include/ember-types.h

remainingTimeSeconds#

uint16_t EmberTransientKeyData::remainingTimeSeconds

Definition at line 2155 of file ./stack/include/ember-types.h

networkIndex#

uint8_t EmberTransientKeyData::networkIndex

Definition at line 2156 of file ./stack/include/ember-types.h