Modules#

Attribute Management

Building and Sending Messages

Endpoint Manipulation

General

Global ZCL

Informational

Network

Security

Test Harness

ZigBee Device Object Commands (ZDO)

Cluster Commands: BACnet Protocol Tunnel

Cluster Commands: Barrier Control

Cluster Commands: Basic

Cluster Commands: Calendar

Cluster Commands: Color Control

Cluster Commands: Configuration Cluster

Cluster Commands: Demand Response and Load Control

Cluster Commands: Device Management

Cluster Commands: Door Lock

Cluster Commands: Events

Cluster Commands: Generic Tunnel

Cluster Commands: Groups

Cluster Commands: IAS ACE

Cluster Commands: IAS Zone

Cluster Commands: Identify

Cluster Commands: Level Control

Cluster Commands: MFGLIB Cluster

Cluster Commands: Messaging

Cluster Commands: On/off

Cluster Commands: Poll Control

Cluster Commands: Power Profile

Cluster Commands: Prepayment

Cluster Commands: Price

Cluster Commands: SL Works With All Hubs

Cluster Commands: Scenes

Cluster Commands: Simple Metering

Cluster Commands: Thermostat

Cluster Commands: Tunneling

Cluster Commands: Window Covering

Plugin Commands for Bulb Pwm Driver

Plugin Commands: APS Link Key Authorization

Plugin Commands: Address Table

Plugin Commands: Antenna

Plugin Commands: BLE

Plugin Commands: Barrier Control Server Cluster

Plugin Commands: Button Joining

Plugin Commands: CLI password protection

Plugin Commands: Calendar Client

Plugin Commands: Calendar Common

Plugin Commands: Calendar Server

Plugin Commands: Coexistence

Plugin Commands: Command Relay

Plugin Commands: Comms Hub Function

Plugin Commands: Comms Hub Function (SubGhz)

Plugin Commands: Compact Logger

Plugin Commands: Concentrator

Plugin Commands: Connection Manager

Plugin Commands: Counters

critical-message-queue Plugin Commands: Critical Message Queue

Plugin Commands: DMP Tuning and Testing

Plugin Commands: Delayed join

Plugin Commands: Demand Response and Load Control

Plugin Commands: Demand Response and Load Control Server

Plugin Commands: Device Database

Plugin Commands: Device Management Client

Plugin Commands: Device Management Server

Plugin Commands: Device Query Service

Plugin Commands: Device Table

Plugin Commands: Door Lock Server Cluster

Plugin Commands: EEPROM

Plugin Commands: EZ-Mode Commissioning

Plugin Commands: Electrical Measurement Server commands

Plugin Commands: End Device Support

Plugin Commands: Events Server

Plugin Commands: Find and Bind Initiator

Plugin Commands: Find and Bind Target

Plugin Commands: Fragmentation

Plugin Commands: GBCS Device Log

Plugin Commands: GBCS Gas Meter

Plugin Commands: Gas Proxy Function

Plugin Commands: Green Power Client

Plugin Commands: Green Power Server

Plugin Commands: Green Power Test Device

Plugin Commands: Green Power Translation Table

Plugin Commands: Groups Server

Plugin Commands: IAS Zone Client

Plugin Commands: IAS Zone Server

Plugin Commands: Identify

Plugin Commands: Idle/Sleep

Plugin Commands: Illuminance Measurement Server commands

Plugin Commands: Interpan

Plugin Commands: Key Establishment

Plugin Commands: MPSI

Plugin Commands: Mac address filtering

Plugin Commands: Manufacturing Library

Plugin Commands: Manufacturing Library CLI

Plugin Commands: Messaging Client

Plugin Commands: Messaging Server

Plugin Commands: Meter Mirror

Plugin Commands: Meter Snapshot Server

Plugin Commands: Multi-Network Price Passthrough

Plugin Commands: Network Creator

Plugin Commands: Network Creator Security

Plugin Commands: Network Find

Plugin Commands: Network Steering

Plugin Commands: OTA Bootload

Plugin Commands: OTA Client

Plugin Commands: OTA Server

Plugin Commands: OTA Simple Storage EEPROM

Plugin Commands: OTA Storage Common

Plugin Commands: PS Store

Plugin Commands: PYD-1698 Occupancy Sensor CLI

Plugin Commands: Partner Link Key Exchange

Plugin Commands: Poll Control Client

Plugin Commands: Power Consumption Model CLI

Plugin Commands: Prepayment Server

Plugin Commands: Price Client

Plugin Commands: Price Common

Plugin Commands: Price Server

Plugin Commands: Relative Humidity Measurement Server commands

Plugin Commands: Relay Control Server

Plugin Commands: Reporting

Plugin Commands: SB1 Gesture Sensor

Plugin Commands: Scenes Server

Plugin Commands: Simple Metering Client

Plugin Commands: Simple Metering Server

Plugin Commands: Simple Metering Server

Plugin Commands: Sleepy Message Queue

Plugin Commands: Slot Manager

Plugin Commands: Smart Energy Registration

Plugin Commands: Stack Diagnostics

Plugin Commands: Standalone Bootloader Client

Plugin Commands: Standalone Bootloader Server

Plugin Commands: Sub-GHz Client

Plugin Commands: Sub-GHz Server

Plugin Commands: Temperature Measurement Server commands

Plugin Commands: Test Harness

Plugin Commands: Throughput

Plugin Commands: Throughput Legacy

Plugin Commands: Trust Center Backup

Plugin Commands: Tunneling Client

Plugin Commands: Tunneling Server

Plugin Commands: Update TC Link Key

Plugin Commands: Wwah Connectivity Manager

Plugin Commands: Wwah Server

Plugin Commands: ZigBee 3.0 Test Harness

Plugin Commands: ZigBee Light Link (ZLL) Commissioning

Plugin Commands: Zigbee Event Logger

Plugin Commands: em4

Utility Commands: Multiple RAIL Demo Code

Application Framework CLI Command Reference#

This header provides cli command function prototypes for the Application Framework's core ZigBee Cluster Library implementation.

Macros#

#define

network form <channel> <power> <panid>

#define

Commands used to change the default link or network key that will be used when forming or joining a network.

#define

Command used for key establishment.

#define

Commands used to send global commands in the zcl.

Macro Definition Documentation#

EMBER_AF_DOXYGEN_CLI__NETWORK_COMMANDS#

#define EMBER_AF_DOXYGEN_CLI__NETWORK_COMMANDS

network form <channel> <power> <panid>

  • Form a network on a given channel, with a given TX Power and PAN ID.

    • channel - uint8_t. The channel on which to form the network.

    • power - int8_t. One byte signed value indicating the TX Power that the radio should be set to.

    • panId - uint16_t. The PAN ID on which to form the network.

network join <channel> <power> <panid>

  • Join a network on a given channel, with a given TX Power and PAN ID.

    • channel - uint8_t. The channel on which to join the network.

    • power - int8_t. One byte signed value indicating the TX Power that the radio should be set to.

    • panId - uint16_t. The PAN ID on which to join the network.

network rejoin <encrypted>

  • Find and rejoin the previous network the device was connected to.

    • encrypted - uint8_t. A single byte boolean 0 or 1 indicating whether or not the rejoin should be done with encryption.

network leave

  • Leave the current network that the device is connected to.

network pjoin <seconds>

  • Turn permit joining on for the amount of time indicated.

    • seconds - uint8_t. A single byte indicating how long the device should have permit joining turn on for. A value of 0xff turns permit join indefinitely.

network broad-pjoin <seconds>

  • Turn permit joining on for the amount of time indicated AND broadcast a ZDO Mgmt Permit Joining request to all routers.

    • seconds - uint8_t. A single byte indicating how long the device should have permit joining turn on for. A value of 0xff turns permit join indefinitely.

network isopen

  • Check if the network has permit joining on and if yes report the remaining time for which the network will be open.

    • seconds - uint8_t. A single byte indicating how long the device will have permit joining turn on for.

network extpanid <bytes>

  • Write the extended PAN ID of the device.

    • bytes - byte array. An array of bytes which represents the extended PAN ID for the device.

network find unused

  • Begins a search for an unused Channel and PAN ID. Will automatically form a network on the first unused Channel and PAN ID it finds.

network find joinable

  • Begins a search for a joinable network. Will automatically attempt to join the first network it finds.


EMBER_AF_DOXYGEN_CLI__SECURITY_CHANGEKEY_COMMANDS#

#define EMBER_AF_DOXYGEN_CLI__SECURITY_CHANGEKEY_COMMANDS

Commands used to change the default link or network key that will be used when forming or joining a network.

changekey link <key>

  • key - 16 byte array. The Link Key provided as a 16 byte array.

changekey network <key>

  • key - 16 byte array. The Network Key provided as a 16 byte array.


EMBER_AF_DOXYGEN_CLI__SECURITY_CBKE_COMMANDS#

#define EMBER_AF_DOXYGEN_CLI__SECURITY_CBKE_COMMANDS

Command used for key establishment.

   <b>cbke start &lt;new partner id&gt; &lt;destination endpoint&gt;</b>
   - new partner ID - uint16_t. The 2 byte node ID of the partner
     with whom to start cbke.

   <b>cbke interpan &lt;pan id&gt; &lt;eui64&gt;</b>
   - PAN ID - uint16_t. The 2 byte PAN ID that the target is located on.
   - eui64 - EmberEUI64. The 8 byte EUI64 of the target (big endian)

   <b>cbke partner &lt;node id&gt; &lt;endpoint&gt;</b>
   - node ID - uint16_t. The two byte node ID of the device
     with whom to initiate key establishment.
   - endpoint - uint8_t. The endpoint on which to begin
     key establishment.

EMBER_AF_DOXYGEN_CLI__ZCL_GLOBAL_COMMANDS#

#define EMBER_AF_DOXYGEN_CLI__ZCL_GLOBAL_COMMANDS

Commands used to send global commands in the zcl.

   <b>zcl global read &lt;cluster&gt; &lt;attribute id&gt; </b>
   - Creates a global read command message to read from
         the cluster and attribute specified.
     - cluster - uint16_t. The cluster id to read from.
     - attribute id - uint16_t. The attribute id to read from

   <b>zcl global write &lt;cluster&gt; &lt;attribute id&gt; &lt;data type&gt; &lt;data&gt;</b>
   - Creates a global write  command message to write to
         the cluster and attribute specified.
     - cluster - uint16_t. The cluster id to read from.
     - attribute id - uint16_t. The attribute id to read from
     - data type - uint8_t. The two byte zigbee type value
     - data - byte array. The data to write

   <b>zcl global uwrite &lt;cluster&gt; &lt;attribute id&gt; &lt;data type&gt; &lt;data&gt;</b>
   - Creates a global write command message to write to the
         cluster and attribute specified.
     - cluster - uint16_t. The cluster id to read from.
     - attribute id - uint16_t. The attribute id to read from
     - data type - uint8_t. The two byte zigbee type value
     - data - byte array. The data to write

   <b>zcl global nwrite &lt;cluster&gt; &lt;attribute id&gt; &lt;data type&gt; &lt;data&gt;</b>
   - Creates a global write command message to write to the
         cluster and attribute specified.
     - cluster - uint16_t. The cluster id to read from.
     - attribute id - uint16_t. The attribute id to read from
     - data type - uint8_t. The two byte zigbee type value
     - data - byte array. The data to write

   <b>zcl global discover &lt;cluster&gt; &lt;attribute id&gt; &lt;max&gt;</b>
   - Creates discovery message for devices with the associated
         cluster and attribute
     - cluster - uint16_t. The cluster id to read from.
     - attribute id - uint16_t. The attribute id to read from
     - max - uint8_t. Max number of discovery responses.

   <b>zcl global report-read &lt;cluster&gt; &lt;attribute id&gt; &lt;direction&gt;</b>
   - Creates a global read reporting command for the associated
         cluster, attribute and server/client direction.
     - cluster - uint16_t. The cluster id to read from.
     - attribute id - uint16_t. The attribute id to read from
     - direction - uint8_t. 0 for client-to-server, 1 for server-to-client.

   <b>zcl global send-me-a-report &lt;cluster&gt; &lt;attribute id&gt; &lt;data type&gt;
      &lt;min report time&gt; &lt;max report time&gt; &lt;reportable change&gt;</b>
   - Creates a global send me a report command for the associated values.
     - cluster - uint16_t. The cluster id for requested report.
     - attribute id - uint16_t. The attribute for requested report.
     - data type - uint8_t. The two byte zigbee type value for the requested report
     - min report time - uint16_t. Minimum number of seconds between reports.
     - max report time - uint16_t. Maximum number of seconds between reports.
     - reportable change - byte array. Amount of change to trigger a report.

   <b>zcl global expect-report-from-me &lt;cluster&gt &lt;attribute id&gt; &lt;timeout&gt;</b>
   - Create a expect-report-from-me message with associated values.
     - cluster - uint16_t. The cluster id for requested report.
     - attribute id - uint16_t. The attribute for requested report.
     - timeout - uint16_t. The maximum amount of time between reports.

   <b>zcl global direction &lt;direction&gt;</b>
   - Sets the direction for global commands, either client to server
         or server to client.
     - direction - uint8_t. The direction for global commands.
       client-to-server == 0, server-to-client == 1.

   <b>zcl global disc-com-gen &lt;start command id&gt; &lt;max command ids&gt;</b>
   - Sends a global Discover Commands Generated command.
     - start command id - uint8_t. The command id to start discovery at.
     - max command ids - uint8_t. The maximum number of command ids to return.

   <b>zcl global disc-com-rec &lt;start command id&gt; &lt;max command ids&gt;</b>
   - Sends a global Discover Commands Received command.
     - start command id - uint8_t. The command id to start discovery at.
     - max command ids - uint8_t. The maximum number of command ids to return.