Plugin Commands: Address Table#
This plugin provides a set of APIs and CLI commands for managing the address table
Macros#
plugin address-table add [entry:8]
plugin address-table lookup [entry:8]
plugin address-table print
plugin address-table remove [entry:8]
plugin address-table set [index:1] [eui64:8] [nodeId:2]
Macro Definition Documentation#
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_ADDRESS_TABLE_PLUGIN_ADDRESS_TABLE_ADD#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_ADDRESS_TABLE_PLUGIN_ADDRESS_TABLE_ADD
plugin address-table add [entry:8]
Add an entry to the address table.
entry - IEEE_ADDRESS - Entry to be added.
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_ADDRESS_TABLE_PLUGIN_ADDRESS_TABLE_LOOKUP#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_ADDRESS_TABLE_PLUGIN_ADDRESS_TABLE_LOOKUP
plugin address-table lookup [entry:8]
Lookup an entry in the address table.
entry - IEEE_ADDRESS - Entry to be looked up.
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_ADDRESS_TABLE_PLUGIN_ADDRESS_TABLE_PRINT#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_ADDRESS_TABLE_PLUGIN_ADDRESS_TABLE_PRINT
plugin address-table print
Prints the address table.
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_ADDRESS_TABLE_PLUGIN_ADDRESS_TABLE_REMOVE#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_ADDRESS_TABLE_PLUGIN_ADDRESS_TABLE_REMOVE
plugin address-table remove [entry:8]
Remove an entry from the address table.
entry - IEEE_ADDRESS - Entry to be removed.
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_ADDRESS_TABLE_PLUGIN_ADDRESS_TABLE_SET#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_ADDRESS_TABLE_PLUGIN_ADDRESS_TABLE_SET
plugin address-table set [index:1] [eui64:8] [nodeId:2]
Set an entry in the address table according to the arguments specified
index - INT8U
eui64 - IEEE_ADDRESS
nodeId - INT16U