Plugin Commands: OTA Server#

The OTA Server plugin provides Over-the-air commands for upgrading firmware and downloading specific files on the server side.

Macros#

#define

plugin ota-server notify [destination:2] [endpoint:1] [payloadType:1] [jitter:1] [manuf-id:2] [imageTypeId:2] [version:4]

#define
#define
#define
#define

plugin ota-server policy page-req-sup [pageRequestSupported:1]

#define
#define
#define

plugin ota-server upgrade [nodeId:2] [endpoint:1] [mfrId:2] [imageType:2] [fileVersion:4]

Macro Definition Documentation#

EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_OTA_SERVER_PLUGIN_OTA_SERVER_NOTIFY#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_OTA_SERVER_PLUGIN_OTA_SERVER_NOTIFY

plugin ota-server notify [destination:2] [endpoint:1] [payloadType:1] [jitter:1] [manuf-id:2] [imageTypeId:2] [version:4]

  • Sends an OTA Image Notify message to the specified destination indicating a new version of an image is available for download.

    • destination - INT16U - The node ID (can be a broadcast address) to which this OTA Notify message should be sent

    • endpoint - INT8U - Target endpoint for the OTA Notify message (only really meaningful for non-broadcast target destination).

    • payloadType - INT8U - Used to specify which parameters you want included in the OTA Notify cluster command payload (0 = jitter value only; 1 = jitter and manufacturer id; 2 = jitter, mfr id, and device id; 3 = jitter, mfr id, device id, and firmware version)

    • jitter - INT8U - Corresponds to QueryJitter parameter in the OTA Upgrade cluster specification. The parameter indicates whether the client receiving Image Notify Command should send in Query Next Image Request command or not.

    • manuf-id - INT16U - Manufacturer ID for the image being advertised (should match the mfr ID in the OTA file's header)

    • imageTypeId - INT16U - Image type ID for the image being advertised (should match the image type ID from the OTA file's header)

    • version - INT32U - Firmware version of the image being advertised (should match the version from the OTA file's header)


EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_OTA_SERVER_PLUGIN_OTA_SERVER_POLICY_BLOCK_REQUEST#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_OTA_SERVER_PLUGIN_OTA_SERVER_POLICY_BLOCK_REQUEST

plugin ota-server policy block-request [policyValue:1]

  • Sets the policy used by the ota-server Policy Plugin when it receives an image block request.

    • policyValue - INT8U - 0: Send block (default), 1: Delay download once for 2 minutes, 2: Always abort download after first block


EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_OTA_SERVER_PLUGIN_OTA_SERVER_POLICY_IMAGE_REQ_MIN_PERIOD#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_OTA_SERVER_PLUGIN_OTA_SERVER_POLICY_IMAGE_REQ_MIN_PERIOD

plugin ota-server policy image-req-min-period [period:2]

    • period - INT16U - The minimum block period in milliseconds.


EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_OTA_SERVER_PLUGIN_OTA_SERVER_POLICY_PAGE_REQ_MISS#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_OTA_SERVER_PLUGIN_OTA_SERVER_POLICY_PAGE_REQ_MISS

plugin ota-server policy page-req-miss [modulus:1]

  • Sets the modulus number of blocks to not respond to. This is used in testing to simulate a device that fails to receive certain blocks from an Image Page Request message.

    • modulus - INT8U - The block modulus number to skip sending when responding to an Image Page Request. E.g. if 2, every other block will not be sent. 0 turns the feature off.


EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_OTA_SERVER_PLUGIN_OTA_SERVER_POLICY_PAGE_REQ_SUP#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_OTA_SERVER_PLUGIN_OTA_SERVER_POLICY_PAGE_REQ_SUP

plugin ota-server policy page-req-sup [pageRequestSupported:1]

  • Sets whether the Page Request feature is supported or not.

    • pageRequestSupported - INT8U - 1 if Page Request is supported, 0 if unsupported


EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_OTA_SERVER_PLUGIN_OTA_SERVER_POLICY_PRINT#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_OTA_SERVER_PLUGIN_OTA_SERVER_POLICY_PRINT

plugin ota-server policy print

  • Prints the polices used by the OTA Server Policy Plugin


EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_OTA_SERVER_PLUGIN_OTA_SERVER_POLICY_QUERY#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_OTA_SERVER_PLUGIN_OTA_SERVER_POLICY_QUERY

plugin ota-server policy query [policyValue:1]

  • Sets the policy used by the OTA Server Policy Plugin when it receives a query request from the client.

    • policyValue - INT8U - 0: Upgrade if server has newer (default), 1: Downgrade if server has older, 2: Reinstall if server has same, 3: No next version (no next image is available for download)


EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_OTA_SERVER_PLUGIN_OTA_SERVER_POLICY_UPGRADE#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_OTA_SERVER_PLUGIN_OTA_SERVER_POLICY_UPGRADE

plugin ota-server policy upgrade [policyValue:1]

  • Sets the policy used by the OTA Server Policy Plugin when it receives an upgrade end request

    • policyValue - INT8U - 0: Upgrade Now (default), 1: Upgrade in 2 minutes, 2: Ask me later to upgrade, 3: Abort Upgrade (send default response)


EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_OTA_SERVER_PLUGIN_OTA_SERVER_UPGRADE#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_OTA_SERVER_PLUGIN_OTA_SERVER_UPGRADE

plugin ota-server upgrade [nodeId:2] [endpoint:1] [mfrId:2] [imageType:2] [fileVersion:4]

  • Instruct a device to upgrade now.

    • nodeId - INT16U - Short destination to send message

    • endpoint - INT8U - Endpoint destination to send message

    • mfrId - INT16U - Manufacturer ID for the image (0xFFFF for wildcard)

    • imageType - INT16U - Image type for the image (0xFFFF for wildcard)

    • fileVersion - INT32U - File version for the image (0xFFFFFFFF for wildcard)