Cluster Commands: MFGLIB Cluster#

This group describes the CLI commands for the MFGLIB Cluster cluster. Listed below is a description of the cluster: This cluster provides commands to kick off MFGLIB actions over the air.

Macros#

#define

zcl mfglib stream [channel:1] [power:1] [time:2]

#define

zcl mfglib tone [channel:1] [power:1] [time:2]

#define

zcl mfglib rx-mode [channel:1] [power:1] [time:2]

Macro Definition Documentation#

EMBER_AF_DOXYGEN_CLI_COMMAND_M_F_G_L_I_B_CLUSTER_STREAM#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_M_F_G_L_I_B_CLUSTER_STREAM

zcl mfglib stream [channel:1] [power:1] [time:2]

  • Command to put the device into streaming mode.

    • channel - INT8U

    • power - INT8S

    • time - INT16U


Definition at line 9254 of file ./app/framework/test/headers/cli.doc

EMBER_AF_DOXYGEN_CLI_COMMAND_M_F_G_L_I_B_CLUSTER_TONE#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_M_F_G_L_I_B_CLUSTER_TONE

zcl mfglib tone [channel:1] [power:1] [time:2]

  • Command to put the device into tone mode.

    • channel - INT8U

    • power - INT8S

    • time - INT16U


Definition at line 9262 of file ./app/framework/test/headers/cli.doc

EMBER_AF_DOXYGEN_CLI_COMMAND_M_F_G_L_I_B_CLUSTER_RX_MODE#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_M_F_G_L_I_B_CLUSTER_RX_MODE

zcl mfglib rx-mode [channel:1] [power:1] [time:2]

  • Command to put the device into RX mode.

    • channel - INT8U

    • power - INT8S

    • time - INT16U


Definition at line 9270 of file ./app/framework/test/headers/cli.doc