Plugin Commands: Update TC Link Key#
The update trust center link key commands are used to manipulate the behavior of the joining device to attempt the trust center link key updates in a certain fashion.
Macros#
#define
plugin update-tc-link-key timer [timeInMilliseconds:4]
Macro Definition Documentation#
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_UPDATE_TC_LINK_KEY_PLUGIN_UPDATE_TC_LINK_KEY_TIMER#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_UPDATE_TC_LINK_KEY_PLUGIN_UPDATE_TC_LINK_KEY_TIMER
plugin update-tc-link-key timer [timeInMilliseconds:4]
This sets the the amount of time between subsequent trust center link key updates in milliseconds.
timeInMilliseconds - INT32U - The amount of time between subsequent trust center link key updates in milliseconds