Plugin Commands: Demand Response and Load Control#
The drlc plugin contributes CLI commands to the application framework to be used for constructing demand response load control commands.
Macros#
plugin drlc clear [endpoint:1]
plugin drlc opt in [endpoint:1] [eventId:4]
plugin drlc opt out [endpoint:1] [eventId:4]
plugin drlc print [endpoint:1]
Macro Definition Documentation#
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_DRLC_PLUGIN_DRLC_CLEAR#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_DRLC_PLUGIN_DRLC_CLEAR
plugin drlc clear [endpoint:1]
Clear the load control event table.
endpoint - INT8U - The relevant endpoint.
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_DRLC_PLUGIN_DRLC_OPT_IN#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_DRLC_PLUGIN_DRLC_OPT_IN
plugin drlc opt in [endpoint:1] [eventId:4]
Modify the entry in the clients load control event table to opt in for a scheduled load control event.
endpoint - INT8U - The relevant endpoint.
eventId - INT32U - The event id of the event that the user is opting in or out of.
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_DRLC_PLUGIN_DRLC_OPT_OUT#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_DRLC_PLUGIN_DRLC_OPT_OUT
plugin drlc opt out [endpoint:1] [eventId:4]
Modify the entry in the clients load control event table to opt out of a scheduled load control event.
endpoint - INT8U - The relevant endpoint.
eventId - INT32U - The event id of the event that the user is opting in or out of.
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_DRLC_PLUGIN_DRLC_PRINT#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_DRLC_PLUGIN_DRLC_PRINT
plugin drlc print [endpoint:1]
Print the Demand Response Load Control Table.
endpoint - INT8U - The relevant endpoint.