Plugin Commands: Antenna#
The antenna commands allow you run-time reconfiguration of the antenna plugin
Macros#
plugin antenna get-active-phy
plugin antenna get-antenna-rx-mode
plugin antenna get-antenna-tx-mode
plugin antenna set-antenna-rx-mode [mode:1]
plugin antenna set-antenna-tx-mode [mode:1]
Macro Definition Documentation#
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_ANTENNA_PLUGIN_ANTENNA_GET_ACTIVE_PHY#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_ANTENNA_PLUGIN_ANTENNA_GET_ACTIVE_PHY
plugin antenna get-active-phy
Get the active RAIL PHY
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_ANTENNA_PLUGIN_ANTENNA_GET_ANTENNA_RX_MODE#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_ANTENNA_PLUGIN_ANTENNA_GET_ANTENNA_RX_MODE
plugin antenna get-antenna-rx-mode
Get the RX antenna mode
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_ANTENNA_PLUGIN_ANTENNA_GET_ANTENNA_TX_MODE#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_ANTENNA_PLUGIN_ANTENNA_GET_ANTENNA_TX_MODE
plugin antenna get-antenna-tx-mode
Get the TX antenna mode
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_ANTENNA_PLUGIN_ANTENNA_SET_ANTENNA_RX_MODE#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_ANTENNA_PLUGIN_ANTENNA_SET_ANTENNA_RX_MODE
plugin antenna set-antenna-rx-mode [mode:1]
Set the RX antenna mode
mode - INT8U - Configure the RX antenna mode(0-don't switch,1-primary,2-secondary,3-RX antenna diversity).
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_ANTENNA_PLUGIN_ANTENNA_SET_ANTENNA_TX_MODE#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_ANTENNA_PLUGIN_ANTENNA_SET_ANTENNA_TX_MODE
plugin antenna set-antenna-tx-mode [mode:1]
Set the TX antenna mode
mode - INT8U - Configure the TX antenna mode(0-don't switch,1-primary,2-secondary,3-TX antenna diversity).