Plugin Commands: Compact Logger#
The compact-logger plugin contributes CLI commands to the application framework to be used for storing information.
Macros#
#define
plugin compact-logger clear
#define
plugin compact-logger set-facility [facility:2]
#define
plugin compact-logger set-severity [severity:1]
Macro Definition Documentation#
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_COMPACT_LOGGER_PLUGIN_COMPACT_LOGGER_CLEAR#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_COMPACT_LOGGER_PLUGIN_COMPACT_LOGGER_CLEAR
plugin compact-logger clear
Clear the log
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_COMPACT_LOGGER_PLUGIN_COMPACT_LOGGER_SET_FACILITY#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_COMPACT_LOGGER_PLUGIN_COMPACT_LOGGER_SET_FACILITY
plugin compact-logger set-facility [facility:2]
Set the facility values messages must meet in order to be logged
facility - INT16U - The new facility value.
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_COMPACT_LOGGER_PLUGIN_COMPACT_LOGGER_SET_SEVERITY#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_COMPACT_LOGGER_PLUGIN_COMPACT_LOGGER_SET_SEVERITY
plugin compact-logger set-severity [severity:1]
Sets the minimum severity level messages must meet in order to be logged
severity - INT8U - The new severity level.