Plugin Commands: Network Creator#
Commands pertaining to network creation with the Network Creator plugin.
Macros#
plugin network-creator form [useCentralizedSecurity:1] [panId:2] [radioTxPower:1] [channel:1]
plugin network-creator mask add [mask:1] [channel:4]
plugin network-creator mask set [mask:1] [newChannelMask:4]
plugin network-creator mask subtract [mask:1] [channel:4]
plugin network-creator start [useCentralizedSecurity:1]
plugin network-creator status
plugin network-creator stop
Macro Definition Documentation#
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_NETWORK_CREATOR_PLUGIN_NETWORK_CREATOR_FORM#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_NETWORK_CREATOR_PLUGIN_NETWORK_CREATOR_FORM
plugin network-creator form [useCentralizedSecurity:1] [panId:2] [radioTxPower:1] [channel:1]
Form a network with specified parameters.
useCentralizedSecurity - BOOLEAN - Whether or not to form a centralized network. If this value is false, the device will attempt to join a distributed network.
panId - INT16U - PanID of the network to be formed
radioTxPower - INT8S - Tx power of the network to be formed
channel - INT8U - channel of the network to be formed
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_NETWORK_CREATOR_PLUGIN_NETWORK_CREATOR_MASK_ADD#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_NETWORK_CREATOR_PLUGIN_NETWORK_CREATOR_MASK_ADD
plugin network-creator mask add [mask:1] [channel:4]
Add a channel to the channel mask of choice.
mask - INT8U - The mask of choice to which to add the channel. Entering an argument of '1' will choose the primary channel mask. Any other argument will choose the secondary channel mask.
channel - INT32U - The channel to add to the channel mask.
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_NETWORK_CREATOR_PLUGIN_NETWORK_CREATOR_MASK_SET#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_NETWORK_CREATOR_PLUGIN_NETWORK_CREATOR_MASK_SET
plugin network-creator mask set [mask:1] [newChannelMask:4]
Set a channel mask.
mask - INT8U - The mask of choice to set. Entering an argument of '1' will choose the primary channel mask. Any other argument will choose the secondary channel mask.
newChannelMask - INT32U - The bit mask to which to set the chosen channel mask.
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_NETWORK_CREATOR_PLUGIN_NETWORK_CREATOR_MASK_SUBTRACT#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_NETWORK_CREATOR_PLUGIN_NETWORK_CREATOR_MASK_SUBTRACT
plugin network-creator mask subtract [mask:1] [channel:4]
Subtract a channel from the channel mask of choice.
mask - INT8U - The mask of choice from which to subtract the channel. Entering an argument of '1' will choose the primary channel mask. Any other argument will choose the secondary channel mask.
channel - INT32U - The channel to subtract from the channel mask.
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_NETWORK_CREATOR_PLUGIN_NETWORK_CREATOR_START#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_NETWORK_CREATOR_PLUGIN_NETWORK_CREATOR_START
plugin network-creator start [useCentralizedSecurity:1]
Starts the network formation process.
useCentralizedSecurity - BOOLEAN - Whether or not to form a centralized network. If this value is false, the device will attempt to join a distributed network.
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_NETWORK_CREATOR_PLUGIN_NETWORK_CREATOR_STATUS#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_NETWORK_CREATOR_PLUGIN_NETWORK_CREATOR_STATUS
plugin network-creator status
Print the status of the network-creator plugin.
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_NETWORK_CREATOR_PLUGIN_NETWORK_CREATOR_STOP#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_NETWORK_CREATOR_PLUGIN_NETWORK_CREATOR_STOP
plugin network-creator stop
Stops the network formation process.