Attribute Management#
Commands related to reading and writing attributes locally on a device.
Macros#
read [endpoint:1] [cluster:2] [attribute:2] [mask:1]
write [endpoint:1] [cluster:2] [attribute:2] [mask:1] [dataType:1] [dataBytes:-1]
Macro Definition Documentation#
EMBER_AF_DOXYGEN_CLI_COMMAND_ATTRIBUTE_READ#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_ATTRIBUTE_READ
read [endpoint:1] [cluster:2] [attribute:2] [mask:1]
Read an attribute from the local attribute table. The attribute is displayed on the command line.
endpoint - INT8U - endpoint of the attribute to read
cluster - INT16U - cluster id of the attribute to read
attribute - INT16U - attribute id of the attribute to read
mask - INT8U - direction mask of the attribute to read (client=0 or server=1)
EMBER_AF_DOXYGEN_CLI_COMMAND_ATTRIBUTE_WRITE#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_ATTRIBUTE_WRITE
write [endpoint:1] [cluster:2] [attribute:2] [mask:1] [dataType:1] [dataBytes:-1]
Write an attribute value into the local attribute table
endpoint - INT8U - endpoint of the attribute to write
cluster - INT16U - cluster id of the attribute to write
attribute - INT16U - attribute id of the attribute to write
mask - INT8U - direction mask of the attribute to write (client=0 or server=1)
dataType - INT8U - the attribute type as listed in the generated file attribute-type.h
dataBytes - OCTET_STRING - string of bytes you wish to write into the attribute table.