Plugin Commands: OTA Client#
The OTA Client plugin provides Over-the-air commands for upgrading firmware and downloading specific files on the client side.
Macros#
plugin ota-client block-test
plugin ota-client bootload [index:1]
plugin ota-client disable-downgrades
plugin ota-client enable-downgrades
plugin ota-client info
plugin ota-client page-request [pageRequest:1]
plugin ota-client pause-at [stopDownloadPercentage:1]
plugin ota-client start
plugin ota-client status
plugin ota-client stop
plugin ota-client upgrade-request
plugin ota-client verify [index:1]
Macro Definition Documentation#
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_OTA_CLIENT_PLUGIN_OTA_CLIENT_BLOCK_TEST#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_OTA_CLIENT_PLUGIN_OTA_CLIENT_BLOCK_TEST
plugin ota-client block-test
Sends an image block request for a file the server should not have. Test harness only (test case 9.5.6 - Missing File)
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_OTA_CLIENT_PLUGIN_OTA_CLIENT_BOOTLOAD#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_OTA_CLIENT_PLUGIN_OTA_CLIENT_BOOTLOAD
plugin ota-client bootload [index:1]
Bootloads the image at the specified index by calling the OTA bootload callback.
index - INT8U - The index at which to begin bootloading the image
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_OTA_CLIENT_PLUGIN_OTA_CLIENT_DISABLE_DOWNGRADES#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_OTA_CLIENT_PLUGIN_OTA_CLIENT_DISABLE_DOWNGRADES
plugin ota-client disable-downgrades
Disable OTA downgrades
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_OTA_CLIENT_PLUGIN_OTA_CLIENT_ENABLE_DOWNGRADES#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_OTA_CLIENT_PLUGIN_OTA_CLIENT_ENABLE_DOWNGRADES
plugin ota-client enable-downgrades
Enable OTA downgrades
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_OTA_CLIENT_PLUGIN_OTA_CLIENT_INFO#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_OTA_CLIENT_PLUGIN_OTA_CLIENT_INFO
plugin ota-client info
Prints the manufacturer ID, Image Type ID, and Version information that are used when a query next image is sent to the server by the client
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_OTA_CLIENT_PLUGIN_OTA_CLIENT_PAGE_REQUEST#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_OTA_CLIENT_PLUGIN_OTA_CLIENT_PAGE_REQUEST
plugin ota-client page-request [pageRequest:1]
pageRequest - INT8U - boolean value turning on (1) or off (0) the page request flag
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_OTA_CLIENT_PLUGIN_OTA_CLIENT_PAUSE_AT#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_OTA_CLIENT_PLUGIN_OTA_CLIENT_PAUSE_AT
plugin ota-client pause-at [stopDownloadPercentage:1]
stopDownloadPercentage - INT8U
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_OTA_CLIENT_PLUGIN_OTA_CLIENT_START#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_OTA_CLIENT_PLUGIN_OTA_CLIENT_START
plugin ota-client start
Starts the ota client state machine. The state machine discovers the OTA server, queries for new images, downloads the images and waits for the server command to upgrade
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_OTA_CLIENT_PLUGIN_OTA_CLIENT_STATUS#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_OTA_CLIENT_PLUGIN_OTA_CLIENT_STATUS
plugin ota-client status
Prints information on the current state of the OTA client download.
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_OTA_CLIENT_PLUGIN_OTA_CLIENT_STOP#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_OTA_CLIENT_PLUGIN_OTA_CLIENT_STOP
plugin ota-client stop
Stops the OTA state machine
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_OTA_CLIENT_PLUGIN_OTA_CLIENT_UPGRADE_REQUEST#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_OTA_CLIENT_PLUGIN_OTA_CLIENT_UPGRADE_REQUEST
plugin ota-client upgrade-request
Send an OTA server an UpgradeEndRequest
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_OTA_CLIENT_PLUGIN_OTA_CLIENT_VERIFY#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_OTA_CLIENT_PLUGIN_OTA_CLIENT_VERIFY
plugin ota-client verify [index:1]
Perform signature verification on the image at the specified index
index - INT8U - The index at which to begin verification of the image