Plugin Commands: Sub-GHz Client#

The Sub-GHz commands provide commands for sub-GHz duty cycle, power management and frequency agility.

Macros#

#define
#define

plugin sub-ghz request-channel-change [nodeId:2] [page:1] [channel:1] [macTxUcastTotal:2] [macTxUcastFailures:2] [macTxUcastRetries:2] [period:1]

Macro Definition Documentation#

EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_SUB_GHZ_CLIENT_PLUGIN_SUB_GHZ_GET_SUSPEND_STATUS#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_SUB_GHZ_CLIENT_PLUGIN_SUB_GHZ_GET_SUSPEND_STATUS

plugin sub-ghz get-suspend-status [nodeId:2] [ep:1]

  • Send the GetSuspendZCLMessagesStatus command to the Sub-GHz server.

    • nodeId - INT16U - Server's node ID

    • ep - INT8U - Server's endpoint


EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_SUB_GHZ_CLIENT_PLUGIN_SUB_GHZ_IGNORE_SUSPEND_STATUS#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_SUB_GHZ_CLIENT_PLUGIN_SUB_GHZ_IGNORE_SUSPEND_STATUS

plugin sub-ghz ignore-suspend-status [ignore:1]

  • Ignore the suspend status when sending ZCL messages (for testing purposes only).

    • ignore - BOOLEAN - Whether or not the suspend status should be ignored


EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_SUB_GHZ_CLIENT_PLUGIN_SUB_GHZ_REQUEST_CHANNEL_CHANGE#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_SUB_GHZ_CLIENT_PLUGIN_SUB_GHZ_REQUEST_CHANNEL_CHANGE

plugin sub-ghz request-channel-change [nodeId:2] [page:1] [channel:1] [macTxUcastTotal:2] [macTxUcastFailures:2] [macTxUcastRetries:2] [period:1]

  • Send the Mgmt_NWK_Unsolicited_Enhanced_Update_notify command to the Sub-GHz server.

    • nodeId - INT16U - Server's node ID

    • page - INT8U - Current channel page

    • channel - INT8U - Current channel

    • macTxUcastTotal - INT16U - Total number of Mac Tx transaction attempts

    • macTxUcastFailures - INT16U - Total number of Mac Tx transaction failures

    • macTxUcastRetries - INT16U - Total number of Mac Tx transaction retries

    • period - INT8U - Time in minutes over which the Mac Tx counts were measured