Plugin Commands: Sleepy Message Queue#

The sleepy-message-queue plugin provides a means to store packets up to a specified period of time.

Macros#

#define

plugin sleepy-message-queue store [timeoutSec:4] [payloadPtr:4] [payloadLength:2] [payloadId:2] [dstEui64:-1]

Macro Definition Documentation#

EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_SLEEPY_MESSAGE_QUEUE_PLUGIN_SLEEPY_MESSAGE_QUEUE_GET_NUM_MSG#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_SLEEPY_MESSAGE_QUEUE_PLUGIN_SLEEPY_MESSAGE_QUEUE_GET_NUM_MSG

plugin sleepy-message-queue getNumMsg [dstEui64:-1]

  • Get the number of pending messages for a given destination EUI64.

    • dstEui64 - OCTET_STRING - The EUI64 of the device for which the number of pending messages is being queried


EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_SLEEPY_MESSAGE_QUEUE_PLUGIN_SLEEPY_MESSAGE_QUEUE_GET_PENDING_MSG#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_SLEEPY_MESSAGE_QUEUE_PLUGIN_SLEEPY_MESSAGE_QUEUE_GET_PENDING_MSG

plugin sleepy-message-queue getPendingMsg [msgId:1]

  • Get the first pending message ID for a given destination EUI64.

    • msgId - INT8U - The messageID of the message to be retrieved.


EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_SLEEPY_MESSAGE_QUEUE_PLUGIN_SLEEPY_MESSAGE_QUEUE_GET_PENDING_MSG_ID#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_SLEEPY_MESSAGE_QUEUE_PLUGIN_SLEEPY_MESSAGE_QUEUE_GET_PENDING_MSG_ID

plugin sleepy-message-queue getPendingMsgId [dstEui64:-1]

  • Get the first pending message ID for a given destination EUI64.

    • dstEui64 - OCTET_STRING - The EUI64 of the device for which the first pending message ID is being queried


EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_SLEEPY_MESSAGE_QUEUE_PLUGIN_SLEEPY_MESSAGE_QUEUE_INIT#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_SLEEPY_MESSAGE_QUEUE_PLUGIN_SLEEPY_MESSAGE_QUEUE_INIT

plugin sleepy-message-queue init

  • Initialize the sleepy message queue.


EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_SLEEPY_MESSAGE_QUEUE_PLUGIN_SLEEPY_MESSAGE_QUEUE_REMAIN_TIME#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_SLEEPY_MESSAGE_QUEUE_PLUGIN_SLEEPY_MESSAGE_QUEUE_REMAIN_TIME

plugin sleepy-message-queue remainTime [msgId:1]

  • Report the remaining timeout on the message specified by the message ID.

    • msgId - INT8U - The messageID of the message whose remaining time will be reported.


EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_SLEEPY_MESSAGE_QUEUE_PLUGIN_SLEEPY_MESSAGE_QUEUE_REMOVE#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_SLEEPY_MESSAGE_QUEUE_PLUGIN_SLEEPY_MESSAGE_QUEUE_REMOVE

plugin sleepy-message-queue remove [msgId:1]

  • Remove the message from the queue with the given messageID.

    • msgId - INT8U - The messageID of the message to be removed.


EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_SLEEPY_MESSAGE_QUEUE_PLUGIN_SLEEPY_MESSAGE_QUEUE_REMOVE_ALL#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_SLEEPY_MESSAGE_QUEUE_PLUGIN_SLEEPY_MESSAGE_QUEUE_REMOVE_ALL

plugin sleepy-message-queue removeAll [dstEui64:-1]

  • Remove all messages from the queue with the given EUI64.

    • dstEui64 - OCTET_STRING - The EUI64 of the device whose messages should be removed.


EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_SLEEPY_MESSAGE_QUEUE_PLUGIN_SLEEPY_MESSAGE_QUEUE_STORE#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_SLEEPY_MESSAGE_QUEUE_PLUGIN_SLEEPY_MESSAGE_QUEUE_STORE

plugin sleepy-message-queue store [timeoutSec:4] [payloadPtr:4] [payloadLength:2] [payloadId:2] [dstEui64:-1]

  • Store a message into the sleepy message queue.

    • timeoutSec - INT32U - Message timeout, in seconds

    • payloadPtr - INT32U - Pointer to (address of) the message payload

    • payloadLength - INT16U - The length of the message payload

    • payloadId - INT16U - The payload ID of this message

    • dstEui64 - OCTET_STRING - The EUI64 of the device to which the message is being sent


EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_SLEEPY_MESSAGE_QUEUE_PLUGIN_SLEEPY_MESSAGE_QUEUE_TIMESTAMP#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_SLEEPY_MESSAGE_QUEUE_PLUGIN_SLEEPY_MESSAGE_QUEUE_TIMESTAMP

plugin sleepy-message-queue timestamp

  • Retrieve the current value of halCommonGetInt32uMillisecondTick().


EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_SLEEPY_MESSAGE_QUEUE_PLUGIN_SLEEPY_MESSAGE_QUEUE_UNUSED_CNT#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_SLEEPY_MESSAGE_QUEUE_PLUGIN_SLEEPY_MESSAGE_QUEUE_UNUSED_CNT

plugin sleepy-message-queue unusedCnt

  • Reads the number of unused queue entries.