Plugin Commands: OTA Storage Common#
The OTA Storage Common plugin provides Over-the-air commands for upgrading firmware and downloading specific files common to both server and client.
Macros#
plugin ota-storage-common data-print [index:1] [offset:4]
plugin ota-storage-common delete [index:1]
plugin ota-storage-common printImages
plugin ota-storage-common reload
plugin ota-storage-common storage-info
Macro Definition Documentation#
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_OTA_STORAGE_COMMON_PLUGIN_OTA_STORAGE_COMMON_DATA_PRINT#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_OTA_STORAGE_COMMON_PLUGIN_OTA_STORAGE_COMMON_DATA_PRINT
plugin ota-storage-common data-print [index:1] [offset:4]
Print arbitray bytes of the OTA image on disk.
index - INT8U - The index of the image to print its data.
offset - INT32U - The offset into the OTA image that will be printed.
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_OTA_STORAGE_COMMON_PLUGIN_OTA_STORAGE_COMMON_DELETE#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_OTA_STORAGE_COMMON_PLUGIN_OTA_STORAGE_COMMON_DELETE
plugin ota-storage-common delete [index:1]
Deletes the image at the specified index.
index - INT8U - The index at which to begin bootloading the image
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_OTA_STORAGE_COMMON_PLUGIN_OTA_STORAGE_COMMON_PRINT_IMAGES#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_OTA_STORAGE_COMMON_PLUGIN_OTA_STORAGE_COMMON_PRINT_IMAGES
plugin ota-storage-common printImages
Prints the images.
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_OTA_STORAGE_COMMON_PLUGIN_OTA_STORAGE_COMMON_RELOAD#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_OTA_STORAGE_COMMON_PLUGIN_OTA_STORAGE_COMMON_RELOAD
plugin ota-storage-common reload
Reload the storage device.
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_OTA_STORAGE_COMMON_PLUGIN_OTA_STORAGE_COMMON_STORAGE_INFO#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_OTA_STORAGE_COMMON_PLUGIN_OTA_STORAGE_COMMON_STORAGE_INFO
plugin ota-storage-common storage-info
Print information about the storage device.