Plugin Commands: Green Power Client#
The Green Power Client plugin contributes CLI commands to the application framework to be used for getting, setting, and displaying information relevant to the Green Power Client cluster.
Macros#
plugin green-power-client add-group-sink [sourceID:4] [sinkGroup:2]
plugin green-power-client add-sink [sourceID:4] [sinkIeee:8]
plugin green-power-client clear-proxy-table
plugin green-power-client duplicate-filter-test [endpoint:1] [sourceId:4] [sequenceNumber:1]
plugin green-power-client print-proxy-table
plugin green-power-client rm-gpd [sourceID:4]
plugin green-power-client rm-sink [sourceID:4] [sinkIeee:8]
plugin green-power-client set-key [index:1] [key:16]
plugin green-power-client set-proxy-entry [index:1] [sourceID:4] [sinkNodeId:2] [options:4]
Macro Definition Documentation#
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_GREEN_POWER_CLIENT_PLUGIN_GREEN_POWER_CLIENT_ADD_GROUP_SINK#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_GREEN_POWER_CLIENT_PLUGIN_GREEN_POWER_CLIENT_ADD_GROUP_SINK
plugin green-power-client add-group-sink [sourceID:4] [sinkGroup:2]
Add a groupcast sink for a given GPD
sourceID - INT32U - GPD Source ID
sinkGroup - INT16U - Sink group
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_GREEN_POWER_CLIENT_PLUGIN_GREEN_POWER_CLIENT_ADD_SINK#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_GREEN_POWER_CLIENT_PLUGIN_GREEN_POWER_CLIENT_ADD_SINK
plugin green-power-client add-sink [sourceID:4] [sinkIeee:8]
Add a sink for a given GPD
sourceID - INT32U - GPD Source ID
sinkIeee - IEEE_ADDRESS - Sink's IEEE address
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_GREEN_POWER_CLIENT_PLUGIN_GREEN_POWER_CLIENT_CLEAR_PROXY_TABLE#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_GREEN_POWER_CLIENT_PLUGIN_GREEN_POWER_CLIENT_CLEAR_PROXY_TABLE
plugin green-power-client clear-proxy-table
clear the proxy table
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_GREEN_POWER_CLIENT_PLUGIN_GREEN_POWER_CLIENT_DUPLICATE_FILTER_TEST#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_GREEN_POWER_CLIENT_PLUGIN_GREEN_POWER_CLIENT_DUPLICATE_FILTER_TEST
plugin green-power-client duplicate-filter-test [endpoint:1] [sourceId:4] [sequenceNumber:1]
This is used to instrument the current device receiving a message in order to test the duplicate message filtering functionality.
endpoint - INT8U
sourceId - INT32U - source Id of the fake incoming message
sequenceNumber - INT8U
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_GREEN_POWER_CLIENT_PLUGIN_GREEN_POWER_CLIENT_PRINT_PROXY_TABLE#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_GREEN_POWER_CLIENT_PLUGIN_GREEN_POWER_CLIENT_PRINT_PROXY_TABLE
plugin green-power-client print-proxy-table
Print the proxy table
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_GREEN_POWER_CLIENT_PLUGIN_GREEN_POWER_CLIENT_RM_GPD#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_GREEN_POWER_CLIENT_PLUGIN_GREEN_POWER_CLIENT_RM_GPD
plugin green-power-client rm-gpd [sourceID:4]
Remove a given GPD from the proxy table
sourceID - INT32U - GPD Source ID
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_GREEN_POWER_CLIENT_PLUGIN_GREEN_POWER_CLIENT_RM_SINK#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_GREEN_POWER_CLIENT_PLUGIN_GREEN_POWER_CLIENT_RM_SINK
plugin green-power-client rm-sink [sourceID:4] [sinkIeee:8]
remove a sink for a given GPD. If that's the last sink, remove the proxy table entry
sourceID - INT32U - GPD Source ID
sinkIeee - IEEE_ADDRESS - Sink's IEEE address
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_GREEN_POWER_CLIENT_PLUGIN_GREEN_POWER_CLIENT_SET_KEY#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_GREEN_POWER_CLIENT_PLUGIN_GREEN_POWER_CLIENT_SET_KEY
plugin green-power-client set-key [index:1] [key:16]
This is used to set the key for a proxy table entry
index - INT8U
key - SECURITY_KEY - source Id of the fake incoming message
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_GREEN_POWER_CLIENT_PLUGIN_GREEN_POWER_CLIENT_SET_PROXY_ENTRY#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_GREEN_POWER_CLIENT_PLUGIN_GREEN_POWER_CLIENT_SET_PROXY_ENTRY
plugin green-power-client set-proxy-entry [index:1] [sourceID:4] [sinkNodeId:2] [options:4]
Set a proxy table entry
index - INT8U - index to proxy table
sourceID - INT32U - GPD Source ID
sinkNodeId - INT16U - Sink's node address
options - INT32U