Plugin Commands: Tunneling Client#
The Tunneling Client Plugin contributes several commands to the application framework's CLI. These commands may be used to create messages related to opening and closing a tunnel between two devices.
Macros#
plugin tunneling-client close [tunnelIndex:1]
plugin tunneling-client print
plugin tunneling-client request [server:2] [clientEndpoint:1] [serverEndpoint:1] [protocolId:1] [manufacturerCode:2] [flowControlSupport:1]
plugin tunneling-client transfer [tunnelIndex:1] [data:-1]
Macro Definition Documentation#
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TUNNELING_CLIENT_PLUGIN_TUNNELING_CLIENT_CLOSE#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TUNNELING_CLIENT_PLUGIN_TUNNELING_CLIENT_CLOSE
plugin tunneling-client close [tunnelIndex:1]
Close a Tunneling cluster tunnel.
tunnelIndex - INT8U - The index of the tunnel to close.
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TUNNELING_CLIENT_PLUGIN_TUNNELING_CLIENT_PRINT#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TUNNELING_CLIENT_PLUGIN_TUNNELING_CLIENT_PRINT
plugin tunneling-client print
Print out the status of active tunnels.
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TUNNELING_CLIENT_PLUGIN_TUNNELING_CLIENT_REQUEST#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TUNNELING_CLIENT_PLUGIN_TUNNELING_CLIENT_REQUEST
plugin tunneling-client request [server:2] [clientEndpoint:1] [serverEndpoint:1] [protocolId:1] [manufacturerCode:2] [flowControlSupport:1]
Request a Tunneling cluster tunnel with a server.
server - INT16U - The network address of the server to which the request will be sent.
clientEndpoint - INT8U - The local endpoint from which the request will be sent.
serverEndpoint - INT8U - The remote endpoint to which the request will be sent.
protocolId - INT8U - The protocol id of the requested tunnel.
manufacturerCode - INT16U - The manufacturer code of the requested tunnel.
flowControlSupport - BOOLEAN - 1 if flow control support is requested or 0 if not.
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TUNNELING_CLIENT_PLUGIN_TUNNELING_CLIENT_TRANSFER#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TUNNELING_CLIENT_PLUGIN_TUNNELING_CLIENT_TRANSFER
plugin tunneling-client transfer [tunnelIndex:1] [data:-1]
Transfer data to a server through a Tunneling cluster tunnel.
tunnelIndex - INT8U - The index of the tunnel through which to send the data.
data - OCTET_STRING - The data to send through the tunnel.