Plugin Commands: Network Steering#
The Network Steering plugin commands are currently being used for the Profile Interop event.
Macros#
plugin network-steering mask add [whichMask:1] [channel:1]
plugin network-steering mask set [whichMask:1] [mask:4]
plugin network-steering mask subtract [whichMask:1] [channel:1]
plugin network-steering pre-configured-key-set [preconfiguredkey:-1]
plugin network-steering start [options:1]
plugin network-steering status
plugin network-steering stop
Macro Definition Documentation#
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_NETWORK_STEERING_PLUGIN_NETWORK_STEERING_MASK_ADD#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_NETWORK_STEERING_PLUGIN_NETWORK_STEERING_MASK_ADD
plugin network-steering mask add [whichMask:1] [channel:1]
Adds a channel to either the primary or secondary channel mask of the network-steering plugin.
whichMask - INT8U - The channel mask to add a channel to.
channel - INT8U - The channel to add to the mask.
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_NETWORK_STEERING_PLUGIN_NETWORK_STEERING_MASK_SET#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_NETWORK_STEERING_PLUGIN_NETWORK_STEERING_MASK_SET
plugin network-steering mask set [whichMask:1] [mask:4]
Set either the primary or secondary channel mask.
whichMask - INT8U - The channel mask to subtract the channel from.
mask - INT32U - The value to set the channel mask to.
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_NETWORK_STEERING_PLUGIN_NETWORK_STEERING_MASK_SUBTRACT#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_NETWORK_STEERING_PLUGIN_NETWORK_STEERING_MASK_SUBTRACT
plugin network-steering mask subtract [whichMask:1] [channel:1]
Subtracts a channel from either the primary or secondary channel mask of the network-steering plugin.
whichMask - INT8U - The channel mask to subtract the channel from.
channel - INT8U - The channel to subtract the mask from.
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_NETWORK_STEERING_PLUGIN_NETWORK_STEERING_PRE_CONFIGURED_KEY_SET#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_NETWORK_STEERING_PLUGIN_NETWORK_STEERING_PRE_CONFIGURED_KEY_SET
plugin network-steering pre-configured-key-set [preconfiguredkey:-1]
Set the pre-configured key
preconfiguredkey - OCTET_STRING - Set the preconfigured key so that the joining device can enter the network.
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_NETWORK_STEERING_PLUGIN_NETWORK_STEERING_START#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_NETWORK_STEERING_PLUGIN_NETWORK_STEERING_START
plugin network-steering start [options:1]
Starts the network steering process.
options - INT8U - A mask of options for indicating specific behavior within the network-steering process.
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_NETWORK_STEERING_PLUGIN_NETWORK_STEERING_STATUS#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_NETWORK_STEERING_PLUGIN_NETWORK_STEERING_STATUS
plugin network-steering status
Displays the current status of the network steering process.
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_NETWORK_STEERING_PLUGIN_NETWORK_STEERING_STOP#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_NETWORK_STEERING_PLUGIN_NETWORK_STEERING_STOP
plugin network-steering stop
Stops the network steering process.