Plugin Commands: Events Server#

The events-server plugin contributes several commands to the application framework's CLI. These commands are be used for adding, clearing, and printing events.

Macros#

#define

plugin events-server add [endpoint:1] [logId:1] [eventId:2] [eventTime:4] [eventData:-1]

#define

plugin events-server clear [endpoint:1] [logId:1]

#define

plugin events-server eprint [endpoint:1] [logId:1] [index:1]

#define

plugin events-server print [endpoint:1] [logId:1]

#define

plugin events-server publish [nodeId:2] [srcEndpoint:1] [dstEndpoint:1] [logId:1] [index:1] [eventControl:1]

#define

plugin events-server set [endpoint:1] [logId:1] [index:1] [eventId:2] [eventTime:4] [eventData:-1]

Macro Definition Documentation#

EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_EVENTS_SERVER_PLUGIN_EVENTS_SERVER_ADD#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_EVENTS_SERVER_PLUGIN_EVENTS_SERVER_ADD

plugin events-server add [endpoint:1] [logId:1] [eventId:2] [eventTime:4] [eventData:-1]

  • Append the event to the event log for the provided endpoint. Once the event log is full, new events will start overwriting old events at the beginning of the table.

    • endpoint - INT8U - the relevant endpoint

    • logId - INT8U - the relevant log

    • eventId - INT16U - the event id

    • eventTime - INT32U - the event time

    • eventData - OCTET_STRING - additional event data


EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_EVENTS_SERVER_PLUGIN_EVENTS_SERVER_CLEAR#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_EVENTS_SERVER_PLUGIN_EVENTS_SERVER_CLEAR

plugin events-server clear [endpoint:1] [logId:1]

  • Clear out the specified event log for the provided endpoint.

    • endpoint - INT8U - the relevant endpoint

    • logId - INT8U - the log to be cleared


EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_EVENTS_SERVER_PLUGIN_EVENTS_SERVER_EPRINT#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_EVENTS_SERVER_PLUGIN_EVENTS_SERVER_EPRINT

plugin events-server eprint [endpoint:1] [logId:1] [index:1]

  • Print the event at the given index in the specified event log for the provided endpoint.

    • endpoint - INT8U - the relevant endpoint

    • logId - INT8U - the relevant log

    • index - INT8U - the index within the event log to print


EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_EVENTS_SERVER_PLUGIN_EVENTS_SERVER_PRINT#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_EVENTS_SERVER_PLUGIN_EVENTS_SERVER_PRINT

plugin events-server print [endpoint:1] [logId:1]

  • Print the specified event log for the provided endpoint.

    • endpoint - INT8U - the relevant endpoint

    • logId - INT8U - the log to be printed


EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_EVENTS_SERVER_PLUGIN_EVENTS_SERVER_PUBLISH#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_EVENTS_SERVER_PLUGIN_EVENTS_SERVER_PUBLISH

plugin events-server publish [nodeId:2] [srcEndpoint:1] [dstEndpoint:1] [logId:1] [index:1] [eventControl:1]

  • Publish an event.

    • nodeId - INT16U - the destination node id

    • srcEndpoint - INT8U - the source endpoint

    • dstEndpoint - INT8U - the destination endpoint

    • logId - INT8U - the relevant log

    • index - INT8U - the index within the event log to set

    • eventControl - INT8U - the event control


EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_EVENTS_SERVER_PLUGIN_EVENTS_SERVER_SET#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_EVENTS_SERVER_PLUGIN_EVENTS_SERVER_SET

plugin events-server set [endpoint:1] [logId:1] [index:1] [eventId:2] [eventTime:4] [eventData:-1]

  • Set the event at the specified index in the event log for the provided endpoint.

    • endpoint - INT8U - the relevant endpoint

    • logId - INT8U - the relevant log

    • index - INT8U - the index within the event log to set

    • eventId - INT16U - the event id

    • eventTime - INT32U - the event time

    • eventData - OCTET_STRING - additional event data