Cluster Commands: BACnet Protocol Tunnel#

This group describes the CLI commands for the BACnet Protocol Tunnel cluster. Listed below is a description of the cluster: Commands and attributes required to tunnel the BACnet protocol.

Macros#

#define

zcl bacnet transfer-npdu random [npdu:1]

Macro Definition Documentation#

EMBER_AF_DOXYGEN_CLI_COMMAND_BACNET_PROTOCOL_TUNNEL_ZCL_BACNET_TRANSFER_NPDU_WHOIS#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_BACNET_PROTOCOL_TUNNEL_ZCL_BACNET_TRANSFER_NPDU_WHOIS

zcl bacnet transfer-npdu whois

  • Send a sample whois command.


Definition at line 881 of file ./app/framework/test/headers/cli.doc

EMBER_AF_DOXYGEN_CLI_COMMAND_B_A_CNET_PROTOCOL_TUNNEL_RANDOM#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_B_A_CNET_PROTOCOL_TUNNEL_RANDOM

zcl bacnet transfer-npdu random [npdu:1]

  • This command is generated when a BACnet network layer wishes to transfer a BACnet NPDU across a ZigBee tunnel to another BACnet network layer.

    • npdu - DATA8


Definition at line 8181 of file ./app/framework/test/headers/cli.doc