Plugin Commands: MPSI#

This plugin provides a set of CLI commands to interact with the MPSI plugin.

Macros#

#define

plugin mpsi receive-message [destinationAppId:1] [messageId:2] [payloadLength:1] [payload:-1]

#define

plugin mpsi send-message [destinationAppId:1] [messageId:2] [payloadLength:1] [payload:-1]

Macro Definition Documentation#

EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MPSI_PLUGIN_MPSI_RECEIVE_MESSAGE#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MPSI_PLUGIN_MPSI_RECEIVE_MESSAGE

plugin mpsi receive-message [destinationAppId:1] [messageId:2] [payloadLength:1] [payload:-1]

  • Simulate receiving an MPSI message.

    • destinationAppId - INT8U - The application ID of the message

    • messageId - INT16U - The message ID of the message

    • payloadLength - INT8U - The payload length of the message

    • payload - OCTET_STRING - The payload of the message. This represents a serialized specific MPSI message.


EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MPSI_PLUGIN_MPSI_SEND_MESSAGE#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MPSI_PLUGIN_MPSI_SEND_MESSAGE

plugin mpsi send-message [destinationAppId:1] [messageId:2] [payloadLength:1] [payload:-1]

  • Simulate sending an MPSI message.

    • destinationAppId - INT8U - The application ID of the message

    • messageId - INT16U - The message ID of the message

    • payloadLength - INT8U - The payload length of the message

    • payload - OCTET_STRING - The payload of the message. This represents a serialized specific MPSI message.