Plugin Commands: CLI password protection#
The CLI-password-protection plugin contributes one command to the application framework's CLI.
Macros#
#define
plugin cli-password-protection changePassword [newPass:4]
Macro Definition Documentation#
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_CLI_PASSWORD_PROTECTION_PLUGIN_CLI_PASSWORD_PROTECTION_CHANGE_PASSWORD#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_CLI_PASSWORD_PROTECTION_PLUGIN_CLI_PASSWORD_PROTECTION_CHANGE_PASSWORD
plugin cli-password-protection changePassword [newPass:4]
This command is used to change the current password.
newPass - INT32U - The new password needs to be a number between 1 and 0xFFFFFFFE