Security#
The Security command set includes all of the commands related to security configuration on the device.
Macros#
changekey link [key:-1]
changekey network [key:-1]
keys delete [index:1]
option install-code [keyTableIndex:1] [ieeeAddress:8] [installCode:-1]
option link [keyTableIndex:1] [ieeeAddress:8] [linkKey:-1]
option register
option security aps off
option security aps on
option security set-allow-trust-center-rejoin-using-well-known-key [allowTrustCenterRejoinUsingWellKnownKey:1]
option security set-allow-trust-center-rejoin-using-well-known-key-timeout [trustCenterRejoinUsingWellKnownKeyTimeout:2]
option security set-key-request-policy [tcLinkKeyRequestPolicy:1] [appLinkKeyRequestPolicy:1]
security mfg-token get
security mfg-token set [magicNumber:4] [value:2]
Commands used for security.
Macro Definition Documentation#
EMBER_AF_DOXYGEN_CLI_COMMAND_SECURITY_CHANGEKEY_LINK#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_SECURITY_CHANGEKEY_LINK
changekey link [key:-1]
Change the link key to the one provided in the 16 byte array argument for this command.
key - OCTET_STRING - The link key provided as a 16 byte array
EMBER_AF_DOXYGEN_CLI_COMMAND_SECURITY_CHANGEKEY_NETWORK#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_SECURITY_CHANGEKEY_NETWORK
changekey network [key:-1]
Change the network key to the 16 byte array provided as an argument to this command.
key - OCTET_STRING - The network key provided as a 16 byte array
EMBER_AF_DOXYGEN_CLI_COMMAND_SECURITY_KEYS_CLEAR#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_SECURITY_KEYS_CLEAR
keys clear
Clear all security keys
EMBER_AF_DOXYGEN_CLI_COMMAND_SECURITY_KEYS_DELETE#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_SECURITY_KEYS_DELETE
keys delete [index:1]
Delete a security key from a given index
index - INT8U - index into the security key table
EMBER_AF_DOXYGEN_CLI_COMMAND_SECURITY_KEYS_PRINT#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_SECURITY_KEYS_PRINT
keys print
Print all security keys out to the command line.
EMBER_AF_DOXYGEN_CLI_COMMAND_SECURITY_OPTION_INSTALL_CODE#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_SECURITY_OPTION_INSTALL_CODE
option install-code [keyTableIndex:1] [ieeeAddress:8] [installCode:-1]
Derives a link key from an install code, sets it in the transient key table for Z3 applications or sets it in the link key table for SE applications.
keyTableIndex - INT8U - index into the link key table
ieeeAddress - IEEE_ADDRESS - IEEE address to enter into the link key table
installCode - OCTET_STRING - install code including two-byte, little-endian CRC
EMBER_AF_DOXYGEN_CLI_COMMAND_SECURITY_OPTION_LINK#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_SECURITY_OPTION_LINK
option link [keyTableIndex:1] [ieeeAddress:8] [linkKey:-1]
Sets a link key in the link key table. Example: option link 0x00 { 06 00 ab 41 64 30 00 0a } {aa bb cc dd ee ff aa bb cc dd ee ff aa bb cc dd}
keyTableIndex - INT8U - index into the link key table
ieeeAddress - IEEE_ADDRESS - IEEE address to enter into the link key table
linkKey - OCTET_STRING - link key to enter into the table
EMBER_AF_DOXYGEN_CLI_COMMAND_SECURITY_OPTION_REGISTER#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_SECURITY_OPTION_REGISTER
option register
Initiates Smart Energy Registration including Key Establishment. This command expects that the device has already joined a smart energy network.
EMBER_AF_DOXYGEN_CLI_COMMAND_SECURITY_OPTION_SECURITY_APS_OFF#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_SECURITY_OPTION_SECURITY_APS_OFF
option security aps off
Turns aps security off
EMBER_AF_DOXYGEN_CLI_COMMAND_SECURITY_OPTION_SECURITY_APS_ON#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_SECURITY_OPTION_SECURITY_APS_ON
option security aps on
Turns aps security on
EMBER_AF_DOXYGEN_CLI_COMMAND_SECURITY_OPTION_SECURITY_SET_ALLOW_TRUST_CENTER_REJOIN_USING_WELL_KNOWN_KEY#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_SECURITY_OPTION_SECURITY_SET_ALLOW_TRUST_CENTER_REJOIN_USING_WELL_KNOWN_KEY
option security set-allow-trust-center-rejoin-using-well-known-key [allowTrustCenterRejoinUsingWellKnownKey:1]
Set whether or not a Trust Center application will allow trust center rejoins for devices using the well-known key.
allowTrustCenterRejoinUsingWellKnownKey - BOOLEAN - Whether or not the Trust Center should allow trust center rejoins for devices using the well-known key.
EMBER_AF_DOXYGEN_CLI_COMMAND_SECURITY_OPTION_SECURITY_SET_ALLOW_TRUST_CENTER_REJOIN_USING_WELL_KNOWN_KEY_TIMEOUT#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_SECURITY_OPTION_SECURITY_SET_ALLOW_TRUST_CENTER_REJOIN_USING_WELL_KNOWN_KEY_TIMEOUT
option security set-allow-trust-center-rejoin-using-well-known-key-timeout [trustCenterRejoinUsingWellKnownKeyTimeout:2]
Sets the number of seconds to allow trust center rejoins for devices using the well-known key. A value of 0 means the policy should not be changed after a timeout. This must be called prior to forming or joining a network.
trustCenterRejoinUsingWellKnownKeyTimeout - INT16U - The number of seconds that trust center rejoins will be responded to using the well-known link key.
EMBER_AF_DOXYGEN_CLI_COMMAND_SECURITY_OPTION_SECURITY_SET_KEY_REQUEST_POLICY#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_SECURITY_OPTION_SECURITY_SET_KEY_REQUEST_POLICY
option security set-key-request-policy [tcLinkKeyRequestPolicy:1] [appLinkKeyRequestPolicy:1]
Sets the local policy for handling TC link key requests and application link key requests. This command sets the emberTrustCenterLinkKeyRequestPolicy and emberAppLinkKeyRequestPolicy attributes. This command should only be entered on the trust center.
tcLinkKeyRequestPolicy - INT8U - The value to assign to emberTrustCenterLinkKeyRequestPolicy
appLinkKeyRequestPolicy - INT8U - The value to assign to emberAppLinkKeyRequestPolicy
EMBER_AF_DOXYGEN_CLI_COMMAND_SECURITY_SECURITY_MFG_TOKEN_GET#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_SECURITY_SECURITY_MFG_TOKEN_GET
security mfg-token get
EMBER_AF_DOXYGEN_CLI_COMMAND_SECURITY_SECURITY_MFG_TOKEN_SET#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_SECURITY_SECURITY_MFG_TOKEN_SET
security mfg-token set [magicNumber:4] [value:2]
magicNumber - INT32U
value - INT16U
EMBER_AF_DOXYGEN_CLI__SECURITY_MFG_TOKEN_COMMANDS#
#define EMBER_AF_DOXYGEN_CLI__SECURITY_MFG_TOKEN_COMMANDS
Commands used for security.
security mfg-token getsecurity mfg-token set <Magic number> <EmberKeySettings value>
Magic number - uint32_t. The 4-byte magic number EMBER_MFG_SECURITY_CONFIG_MAGIC_NUMBER to prevent accidental execution.
EmberKeySettings value - uint16_t. The 2-byte value for EmberKeySettings indicating key permissions.