The internal representation of a proxy or sink table entry.
Public Attribute Documentation#
status#
EmberGpProxyTableEntryStatus EmberGpProxyTableEntry::status
Internal status. Defines if the entry is unused or used as a proxy entry
options#
uint32_t EmberGpProxyTableEntry::options
The tunneling options (this contains both options and extendedOptions from the spec)
gpdSecurityFrameCounter#
EmberGpSecurityFrameCounter EmberGpProxyTableEntry::gpdSecurityFrameCounter
The SFC of the GPD
sinkList#
EmberGpSinkListEntry EmberGpProxyTableEntry::sinkList[GP_SINK_LIST_ENTRIES]
The list of sinks (hardcoded to 2 which is the spec minimum) (maybe we should indirect this?)