Describe the Initial Security features and requirements that will be used when forming or joining ZigBee Light Link networks.
Public Attributes#
uint32_t
Public Attribute Documentation#
bitmask#
uint32_t EmberZllInitialSecurityState::bitmask
This bitmask is unused. All values are reserved for future use.
keyIndex#
EmberZllKeyIndex EmberZllInitialSecurityState::keyIndex
The key encryption algorithm advertised by the application.
encryptionKey#
EmberKeyData EmberZllInitialSecurityState::encryptionKey
The encryption key for use by algorithms that require it.
preconfiguredKey#
EmberKeyData EmberZllInitialSecurityState::preconfiguredKey
The pre-configured link key used during classical ZigBee commissioning.