Debug Print#
API and Callbacks for the Debug Print Component.
API#
sl_zigbee_debug_print_enable_group(uint32_t group_type, bool enable)
void
sli_zigbee_debug_print_buffer(uint32_t group_type, const uint8_t *buffer, uint16_t buffer_length, bool with_space, const char *format_string)
Enumerations#
enum
SL_ZIGBEE_DEBUG_PRINT_TYPE_STACK = 0x01
SL_ZIGBEE_DEBUG_PRINT_TYPE_CORE = 0x02
SL_ZIGBEE_DEBUG_PRINT_TYPE_APP = 0x04
SL_ZIGBEE_DEBUG_PRINT_TYPE_ZCL = 0x08
SL_ZIGBEE_DEBUG_PRINT_TYPE_LEGACY_AF_DEBUG = 0x10
}
Macros#
#define
local_printf printf
#define
local_vprintf vprintf
#define
#define
#define
#define
#define
#define
#define
#define
#define
#define
#define
#define
#define
#define
#define
#define
#define
#define
#define
#define
API Documentation#
sl_zigbee_debug_print_enable_group#
sl_status_t sl_zigbee_debug_print_enable_group (uint32_t group_type, bool enable)
Parameters
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint32_t | N/A | group_type | Ver.: always |
| bool | N/A | enable | value Ver.: always |
Enable groups in debug prints.
Returns
sl_status_t status code
sli_zigbee_debug_print_buffer#
void sli_zigbee_debug_print_buffer (uint32_t group_type, const uint8_t * buffer, uint16_t buffer_length, bool with_space, const char * format_string)
Parameters
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint32_t | N/A | group_type | Ver.: always |
| const uint8_t * | N/A | buffer | value Ver.: always |
| uint16_t | N/A | buffer_length | |
| bool | N/A | with_space | |
| const char * | N/A | format_string |
Enable groups in debug prints.
Returns
sl_status_t status code
Enumeration Documentation#
sl_zigbee_debug_print_type#
sl_zigbee_debug_print_type
| Enumerator | |
|---|---|
| SL_ZIGBEE_DEBUG_PRINT_TYPE_STACK | |
| SL_ZIGBEE_DEBUG_PRINT_TYPE_CORE | |
| SL_ZIGBEE_DEBUG_PRINT_TYPE_APP | |
| SL_ZIGBEE_DEBUG_PRINT_TYPE_ZCL | |
| SL_ZIGBEE_DEBUG_PRINT_TYPE_LEGACY_AF_DEBUG | |