Modules#
WWAH App Event Retry Manager#
API and Callbacks for the WWAH App Event Retry Manager Component.
Silicon Labs proprietary Works With All Hubs (WWAH) app event retry manager.
API#
Write attribute-enabled callback.
Write attribute queue size callback.
WWAH app event retry manager set backoff parameters to default.
API Documentation#
emberAfPluginWwahAppEventRetryManagerWriteAttributeEnabled#
void emberAfPluginWwahAppEventRetryManagerWriteAttributeEnabled (uint8_t enabled)
Write attribute-enabled callback.
Type | Direction | Argument Name | Description |
---|---|---|---|
uint8_t | N/A | enabled | Ver.: always |
This callback is called when the enabled backoff parameter is changed.
emberAfPluginWwahAppEventRetryManagerWriteAttributeQueueSize#
void emberAfPluginWwahAppEventRetryManagerWriteAttributeQueueSize (uint8_t queueSize)
Write attribute queue size callback.
Type | Direction | Argument Name | Description |
---|---|---|---|
uint8_t | N/A | queueSize | Ver.: always |
This callback is called when the app event retry queue size is being reported.
emberAfWwahAppEventRetryManagerSetBackoffParamsToDefault#
void emberAfWwahAppEventRetryManagerSetBackoffParamsToDefault (void )
WWAH app event retry manager set backoff parameters to default.
Type | Direction | Argument Name | Description |
---|---|---|---|
void | N/A |
This callback is called when the app event retry manager is about to set the backoff parameters of the critical message queue provider plugin back to their default.